Browse FAQs



Data Center Expert | How do hardware and software support contracts work?
... hardware warranty and software support contracts work for StruxureWare Data Center Expert. StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... Software Support Contract StruxureWare Data Center Expert appliances come ... software support . The Data Center Expert appliance and ... active and complete software support in order to ... technical support and software upgrades. Software support contracts are required for ... covered under base software support SKUs) as ... ... not currently require support contracts . Hardware Support Contracts StruxureWare Data Center Expert Appliances can ... Hardware support must be continuous ... Year 1
NetBotz | Hardware & Software Support Information and Limits
... Hardware Warranty & Software Support The NetBotz Rack Appliances 750 has a software /hardware support limitation of 5 ... Year 1 Year 2 Year ... 5 Year 6 Software Support & Hardware Support Factory Warranty Out of Support Out of Support The NetBotz Rack Appliances 250 has a software /hardware support limitation of 5 ... Year 1 Year 2 Year ... 5 Year 6 Software Support & Hardware Support Factory Warranty Out of Support Out of Support The NetBotz Rack Appliances 355 and 455 have a software /hardware support limitation of 5 ... ... base 2 year software support contract must be purchased ...
APC Security Advisory - InfraStruxure Central 5.0 Java Runtime Environment
... processing of XML Data . [ 1 ] ... processing of XML data may allow unauthorized ... ... with processing XML data may allow an untrusted applet or application that is downloaded ... ... of malicious XML data ... uploading of XML data , the data must adhere to ... ... untrusted applet or application to elevate its ... ... or execute local applications that are accessible ... ... Central Client uses one font throughout all ... ... Environment Scripting Language Support . ... to scripting language support may allow an untrusted applet or application to elevate its ... ... or execute local applications that are accessible ...
Did APC purchase the AirFlow Company?
Data Center Cooling American Power Conversion Expands Availability Solutions with Acquisition of Airflow Company ... , global, one -stop shop ... ... specifically designed for applications that are sensitive ... IT and telecommunications applications . ... a variety of applications including datacenters, ... ... solutions also offer one of the smallest ... ... and Advance Power’s operations ; the timely ... of global manufacturing capacity ; general worldwide ... ... equipment, related software , professional and ... APC, which is headquartered in West Kingston, Rhode Island, reported sales of $ 1 .337 billion for the year ended December 31, 1999 and is a Fortune 1000 and S&P 500 company.
DAC, Cancoil Installation Manual
... This document contains information on how to ... Section 1 . Warranty and General Information ……… ... ... and Sequence of Operations ……… ... ... Cooled Condensers For information pertaining to product ... and electrical and capacity data , please visit ... Section 1 . General Information ... efficient year round operation for low, ... high temperature refrigeration applications . ... A minimum of 1000 cfm (of ... ... record the following information in the space ... The following information may be used ... The data in the tables ... ... are based on 1 degree per 100 ... Suction riser capacity is the MINIMUM ...
APC Security Advisory - Static Factory Password Vulnerability
... or device has one of these cards ... ... manual for further information . ... to a newer application revision that has ... at the same application revision for those ... ... devices with network support are affected. ... Description AOS Rev APP Rev AOS Rev APP Rev Smart- ... ... mx28 110 Switched Rack PDU aos 116 ... ... The AOS and APP firmware revisions listed ... ... _hw02_ APP _REV. ... ... both AOS and APP revsions are available ... ... Description AOS Rev APP Rev AOS Rev APP Rev Smart- ... ... The AOS and APP firmware revisions listed ... ... or device has one of these cards ...
Video: How do I configure APC Network Management Card network settings?
... Environmental Monitoring Unit 1 (AP9312TH) ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... ... Network Management Card 1 : ... Network Management Card 1 (AP9617, ... Network Management Card 1 (such as ... AP78XX or AP79XX Rack PDU, Environmental ... ... Network Management Card 1 based devices are ... ... AP8XXX Next Gen Rack PDU (NMC2 ... ... device, select one of the available ...
INFORMATION BULLETIN: Potential Issue with AP8XXX series Rack Power Distribution Units with rpdu2g v6.0.9 firmware
... , the rest of the firmware modules (AOS, rpdu2g application module) need to be loaded by one of the methods available here ...
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
3. Run a terminal program such as HyperTerminal ... bps, 8 data bits, no parity, 1 stop bit, and no flow ...
Network Management Card (NMC) Password Reset Procedure
... Environmental Monitoring Unit 1 (AP9312TH) ... Network Management Card 1 - AP9617, ... ... Network Management Card 1 include (but ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... ... Network Management Card 1 Procedure 1 .) ... Network Management Card 1 -enabled device ... Rack PDU (AP84XX ... 1st Generation Rack Automatic Transfer Switch ... 940- 1000 (DB- ... 2nd Generation Rack Automatic Transfer Switch ... 4th Generation Rack Automatic Transfer Switch ... Rack Air Removal Unit ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.