SYTF2 for use with Symmetra RM with 208vac Input and Output only
Symmetra Step-Down Transformers ... windings of this transformer , he NEMA ... ... this voltage from 208v AC to 120v AC. ... other voltage then 208v . ... BYPASS Mode the UPS will not be ... If the UPS has 240vac on the input side and is put into Bypass mode, it will then pass that voltage through the UPS to the output. This will cause the SYTF2 to be receiving 240vac and therefore it will only be able to step it down to approximately 139VAC.