Technical FAQs

Ask a Question

Are there any 600mm units that have return air temperature limits for warranty purposes?

Issue:  
Are there any 600mm units that have return air temperature limits for warranty purposes?

Product line:
ACRP1XX, ACRP5XX, ACRD5XX, ACRD5XX.

Environment:  
All Serial Numbers.

Cause:
Install, Repair.

Resolution:
There are inlet temperature limits of 113 degrees F. This temperature is driven from maximum limits of accessory and support products and to maintain suction gas temperatures within acceptable range on the DX units.
 
 
 
 
Was this helpful?
What can we do to improve the information ?