Pesquisar Perguntas frequentes



Hardwiring to 120v, 208v, and 240v loads from a 208v/240v SmartUPS RT UPS
... down transformers, APC manufactures 4 larger ... ... To supply a 120 v load, the ... 2 120 volt legs that ... ... 240 v/ 120 v panel where there ... 2 legs of 120 v and from hot ... ... To supply a 208 v load, the ... 120 v Hot Leg ... phase from the 120 v leg) ... you would measure 208 volts from Hot ... ... legs that are 120 degrees out of ... A split phase UPS will require a 4 wire input and will output 2 balanced 120 v legs, a ground, and a neutral.
Single Phase Symmetra Drops the Load When Returning from Bypass
Input Voltage: Line I 132.7, Line II 132.7, LI-LII 230 VAC Output Voltage Setting: 208 V
How do I update the firmware of my SRT, SMC, XU, XP, SMX, SMT, SMTL, SCL, SRC, CHS series Smart-UPS?
Devices that do *NOT* have upgradable firmware: These units are 120 V devices built prior to date code 1037. Date code is the first 4 numbers in your serial number.
How do I update the firmware of my SRT/SMC/XU/XP/SMX/SMT/SCL/SRC/CHS series Smart-UPS using the Firmware Upgrade Wizard?
Issue: These units are 120 V devices built prior to date code 1037. Date code is the first 4 numbers in your serial number.
Video: How do I configure a 208v Smart-UPS RT or SRT for use with a 240v input?
If you need 120 v for your equipment you will still need to use a stepdown transformer.
What are the basic troubleshooting steps for the Smart-UPS smx1500rm2u ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smx2000hv / smx3000hv ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smx2000lv / smx3000lv ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smc1000 / smc1500 ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smx2000rmhv2u / smx3000rmhv2u ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)


Resultados 1 - 10 de 64

Não encontra o que procura?

Contacte a nossa equipa de apoio ao cliente para receber informações sobre assistência técnica, assistência relativamente a reclamações e muito mais.