DAC, Cancoil Installation Manual
... ... 3 Section 3 . Wiring and ... ... designed to provide years of reliable performance ... stable, efficient year round operation for ... high temperature refrigeration applications . Allow 3 feet of clearance ... ... servicing and preventative maintenance . Section 3 . Electrical Wiring ... ... followed at all times to prevent venting ... 3 . Verify the ... ... for a particular application or specific location ... ... before service or maintenance to determine which ... ... in response to changes in the outdoor ... During periods of warm outdoor temperature, the liquid returns to the refrigerant receiver, and the condenser returns to full capacity.