Pesquisar Perguntas frequentes



How To: Configuring an APC Network Management Card with popular email services such as Gmail, Yahoo!, Office 365, and Hotmail/Outlook.com
Devices with an embedded Web/SNMP Card include (but are not limited to): Environmental Monitoring Unit 1 (AP9312TH)
Can I use multiple ACSC1XX units in a single room?
Issue: This article answers the question of can I use multiple ACSC1XX units in a single room ?
How to set up group communications for an Network Air FM unit
... Network Air FM unit . ... group of FM units to work together ... ... independent, Computer Room Air Conditioner. ... a set of one to three Modules ... ... together as a single unit and up to ... ... In a system one of the modules ... ... backup systems to service the load properly ... ... System Failures for one system do not ... be the same ones for other systems ... 1 ) Please locate ... of the FM unit [Figure 1 ] and land ... connects the next unit in the group ... 1 Figure ... . Please select one of these configurations ... ... number of FM units in the system ...
How to navigate through an Network Air FM unit display
... Network Air FM unit display. Only qualified service personnel should make ... ... humidity of the room air. ... point in the room . If the room temperature is 23 ... ... point of the room is 26° ... ... between the actual room dew point and the desired room dew ... to control the room environment or if ... ... work as a single System. ... Half capacity uses one compressor and half ... Rooms with small heat ... When the unit is in dehumidification ... ... compressor (stage 1 ) in a ... ... sequentially in your room after a power ... ... reading of the room conditions and it ...
Guidelines for installation of an acsc100, or acsc101
Room preparation ... . Ensure the room is insulated to ... room must be sealed ... The room should be thoroughly ... room should have a ... ... airflow for each unit supported. ... of heat per unit . Receiving the unit ... Your InRow SC unit has been factory ... ... have received the unit in excellent condition ... crating and the unit immediately upon receipt ... ... the APC technical service department at 1 -888- ... The unit is manufactured with ... maximum strength and unit integrity. However ... as with all electrical and mechanical equipment, you must take care with proper rigging of your unit . ... using a forklift, move the unit on the shipping pallet only.
How to read a pressure temperature chart for super-heat and sub-cooling calculations
... All DX Cooling units . ... valuable tool that service technicians use to ... Single -component refrigerants ... and condense at one temperature for a ... ... Therefore, only one column is needed ... (see Figure 1 ) ... , more of one component will transfer ... ... of temperature from one side of the ... ... defined by a single pressure-temperature ... Imagine a room full of vapor ... ... each temperature: one for the saturated ... ... only separated by 1 or 2 psi ... ... will only list one column for these ... ... as for a single -component refrigerant ... For a single -component or ...
Can I change the input plug or reduce the cord length on my Rack Power Distribution Unit (Rack PDU) or Rack Automatic Transfer Switch (ATS)?
... acceptability of the modification or if the modifications are significant enough to require one of UL's Field Engineering Services staff members to evaluate the modified ...
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
... PDU, AV unit , or environmental monitoring unit with an embedded ... ... : Environmental Monitoring Unit 1 (AP9312TH) ... ... Network Management Card 1 - AP9617, ... ... Network Management Card 1 include (but ... , Environmental Monitoring Units (ap9320, ... ... firmware to take advantage of enhancements, ... Symmetra 1 phase (Symmetra ... ... Management Card 2 units with the SKU ... ... Network Management Card 1 and 2 ... Network Management Card 1 and 2 ... Network Management Card 1 and 2 ... Network Management Card 1 and 2 1 . Obtain the ... ... Network Management Card 1 and 2*
acpa4000 Spare Parts List
... Rear of the unit ... ROTARY 115/ 1 /60 ( ... ... (CAT2P16S3R126B- 1 A) ... FT X 8 IN ... BYPASS ADRI- 1 - 1 _4- ... ... ducts to the unit and ceiling ... BULKHEAD MOUNT ( single float ... rear of the unit ) (az2280- 1 C-120a) 450-0001 Replacement Breaker ( Unit Circuit Breaker ... AP9512THBLK TEV SPORLAN BBIVE- 1 -cp100-b20 (BBIVE- 1 -cp100-b20 875-4199A TUBE TWIN INSERT 1 /8" (O-ring ... 0w0436 Services Description: ... 1 Year Extended Warranty for NetworkAir acpa4000 (WEXTWAR1YR-AX-12)
Rack PDU 2G (AP8XXX) Network Port Sharing Information
... ability to share one IP address via one network connection) ... PDUs using only one ... , 5. 1 .6 or ... ... a number, 1 to 4, ... ... are connected to one another in a ... ... in the unused IN /OUT ports ... ... in either the IN or OUT port ... ... " port of one of the grouped ... This unit will be the ... ... powering up the units for the first ... desired order, 1 to 4. ... ... power up the unit that you would ... have Display ID 1 .


Resultados 1 - 10 de 90

Não encontra o que procura?

Contacte a nossa equipa de apoio ao cliente para receber informações sobre assistência técnica, assistência relativamente a reclamações e muito mais.