Video: Data Center Expert | Managing Users
4 ) Click the ... 4 ) Click OK 4 ) Confirm the ... 4 ) Select 4 ) Click Add ... 4 ) Click Edit ... 4 ) Select ... 4 ) Click Delete ... Issues Binding to Search Base that Contains an Object starting with # ... - AD objects that begin with a # can cause parsing issues within DCE. ... Typically binding to a Search Base one container higher than the one that contains the object beginning with '#' will resolve the issue. ... The only current work around is that the users can be individually added into Data Center Expert via Active Directory, instead of using Groups.