{}

Pesquisar perguntas frequentes

{"searchBar":{"inputPlaceholder":"Pesquisar por palavra-chave ou fazer uma pergunta","searchBtn":"Pesquisar","error":"Insira a palavra-chave que deseja pesquisar"}}

PowerChute Network Shutdown cannot be installed on 32-bit systems

Issue:
PowerChute Network Shutdown v4.3 and higher (v4.3+) cannot be installed on 32-bit systems.

Product Line:
PowerChute Network Shutdown

Environment:
All supported OS

Cause:
PowerChute v4.3 is bundled with JDK 11, which does not support 32-bit systems.

Solution:
If you require PowerChute on a 32-bit system, install PowerChute Network Shutdown v4.2, which is the last version to support 32-bit systems. To download PowerChute v4.2, visit the PowerChute Network Shutdown Product Page.

Isto foi útil?

Conheça mais
Conheça mais