Pesquisar perguntas frequentes
AP9613 Status LED Behavior Explanation
Issue
What does the LED indicator on the AP9613 Dry Contact I/O SmartSlot card indicate?
Product Line
- UPS Device Management
- AP9613 Dry Contact I/O SmartSlot Card
Environment
- v101 firmware
- All serial numbers
Cause
The current status LED behavior is for reference and to clarify what is in the user's guide. Refer to the information below.
Resolution
State | LED Indicator |
AP9613 is booting or starting up | Flashing/Blinking Green |
UPS Communication Error/Lost Communication with UPS | Flashing/Blinking Red |
Universal I/O (UIO) error and/or Lost Communication with UIO Accessory | |
AP9613 Hardware Error | |
Configuration Error - Invalid configuration file on the AP9613 | Rapid Flashing/Blinking Red |
UPS "Fault" (as outlined in knowledge base FA171541) | Solid Red |
Normal Operation | Solid Green |
In order to verify the status of the AP9613 and it's configuration, the Dry Contact I/O SmartSlot Configuration Utility can be accessed via the USB connection as per the instructions in the user's guide.