Consultar las preguntas frecuentes



Smart-UPS C Series FAQ
Smart-UPS C Series FAQ Smart-UPS ... is the new Smart-UPS C series? The Smart-UPS C series is ... new entry level Smart-UPS product designed for ... ... feature a new LCD Interface. ... dedicated Tower or Rack -Mount models ... 1000 VA and 1500 VA capacities. ... 1500va in both Rack and Tower form ... ... America use NEMA 5 -15 plugs ... ... with the SMC Smart-UPS ? The SMC Smart-UPS supports Powerchute Business ... ... not have a Smart -Slot and ...
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
UPS Network Management Card v3. X . X Firmware for Smart-UPS and Matrix w/AP9617/8/9 installed or
Video: How do I configure APC Network Management Card network settings?
Return to Top Configuration Method 5 - via Smart-UPS front panel LCD - (Supported SMT, SMX, and SRT
What are the various generations of Smart-UPS Products?
... of single phase Smart-UPS Products? Smart-UPS ... a variety of Smart-UPS products in use ... ... Over the years APC has steadily improved ... ... refer to the apc .com product ... for your specific UPS . Current Products: ... generation Line Interactive Smart-UPS products Fully interactive LCD display ... Serial Port on UPS ) Smart -Slot for installation of APC Accessory Cards ... generation Line Interactive Smart-UPS products Fully interactive LCD display All units Rack / Tower convertible Voltage adaptability ( 2kva ... ... Serial Port on UPS ) Smart -Slot for installation of APC Accessory Cards
How can I adjust the number of battery packs on a Smart-UPS XL?
Smart-UPS XL products require ... you tell the UPS how many external ... so that the UPS can properly calculate ... Smart-UPS XL ... runtime and have Smart Batteries. Smart-UPS XL models are ... Smart-UPS XL models are ... ... calculations which a Smart-UPS performs when it ... ways program the Smart-UPS XL to recognize ... ... . First, EXIT out of the ... the UPS service must be ... 5 . Click on ... ... properly with an APC UPS or ... com port the UPS serial ... PowerChute plus version 5 . x for Windows 95 ...
Why might the LEDs on my Back-UPS or Smart-UPS SC be flashing?
... LS, and Smart-UPS SC: causes ... ... UPS NS/ XS /RS, Smart-UPS SC 620va and ... ... indicates that the UPS is performing a ... ... indicates that the UPS has entered " ... " where the UPS will turn off ... The UPS is put into ... ... Guide) your ups may "" ... ... "" your UPS , press the ... ... indicates that the UPS is operating normally ... ... indicates that your UPS is operating on ... The UPS can only provide ... If your UPS is operating on ... ... mind that the UPS will run on battery whenever UPS deems the power ...


Resultados 1 - 10 de 64

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.