Consultar las preguntas frecuentes



How do I upgrade and activate premium devices in StruxureOn?
... .4. X When you start using the StruxureOn ... About Premium 24 / 7 expert monitoring of your data center The Schneider Electric Service Bureau will remotely monitor all connected physical infrastructure devices 24 hours a day, 7 days a week enabling remote troubleshooting for quick resolution of critical incidents. ... Proactive service dispatch ... To upgrade a device The first time you upgrade one or more devices, you must read about pricing and accept the license agreement to continue.
Video: Silent Installation of a Windows PowerChute Business Edition Agent versions 7.x - 9.2.1
Launch a command prompt by selecting the Windows start button and then Run
PowerChute Personal Edition v3.X Error Code 2738 – Unable to install the software.
... v3. X Error Code 2738 ... ... Edition 3. X . ... Edition 3. X . ... Vista and Windows 7 operating system and ... ... · Click on Start -> All ... ... · Click on Start -> All ... Considering that, plus the fact that SFC /scannow is completely automatic and very easy to use, the tool should usually be one of your first troubleshooting steps. 1. Click Start , click All Programs, click Accessories, right-click Command Prompt, and then click Run as administrator. ... A message will appear stating that The system scan will begin .
Data Center Expert | Application Version does not update in the UI after upgrading devices to AOS 6.4.6 and newer
StruxureWare DCE 7 . X ... This problem is caused by a firmware enhancement on NMC2 devices beginning with AOS 6.4.6 and newer.
"Updates are available" pop up messages appear after upgrading PowerChute Personal Edition to version 3.0.2
If you are seeing updates are available pop up messages appearing after upgrading PowerChute Personal Edition 3. X to version 3.0.2 this indicates that the APC Data Service has been stopped. ... To resolve the issue restart the APC Data Service . On Windows Vista and Windows 7 go to Control Panel > Administrative Tools > Services Double click on APC Data Service and select start .
Video: How to reset the PowerChute Network Shutdown password and user name.
PowerChute Network Shutdown v3. X and 4. X ... 1. Stop the PowerChute service . ... 7 . Start the PowerChute service and log in with your new username and password.
Security Notification: "LOGJAM" vulnerability (CVE-2015-4000) - impact to PowerChute Network Shutdown.
... .2. x – These versions ... ... .0. x – DHE_ ... Java 7 may use 768 ... Java 7 may use 768 ... ... OS, Java 7 must be used ... ... .2. x – Install the ... ... .2. x will automatically detect ... V3.0. x – Install the 32-bit version of Java 8 from java.com on the machine running PowerChute. ... Once PowerChute has been configured to use Java 8 (Java 7 on Solaris x86): Stop the PowerChute service . ... Save the file and re- start the PowerChute service .
PowerChute Network Shutdown Virtual Appliance Hostname resets after reboot
PowerChute Network Shutdown Appliance 4. x &3. x ... Must stop or restart the PCNS service for the host name to change in the PCNS web interface. The commands are service PowerChute stop and service PowerChute start . ... 7 . Click OK to close the window
Migrate PowerChute Network Shutdown configuration from PowerChute v4.2, v4.3 virtual appliance to v4.4 virtual appliance
... .2 CentOS 7 virtual appliance, ... .3 CentOS 7 virtual appliance, ... For information, see the Log in as root and stop the PowerChute service : 2. Log in as root and stop the PowerChute service : ... stop PowerChute. service ... 3. Log in and stop the PowerChute service : ... 4. Save the below v4. x configuration files locally from the /opt/APC/PowerChute/group1 directory: ... 7 . Edit the pcnsconfig.ini ... 9. Start the PowerChute service : ... start PowerChute. service
Video: How do I configure APC Network Management Card network settings?
... MAC address that begin with 00 C0 B 7 ... version 3. x . x or higher. ... any MAC addresses beginning with 00 C0 B 7 , which indicates ... ... program, any services using the COM ... ... the APC UPS service must be stopped ... ... correct cable, start the terminal emulation ... ... .0. X . ... .0. X On Mac OS X specifically: sudo ... Mac OS X command format: ... Beginning with the AOS 5.1.5 release, the NMC2 has implemented Option 12 (Host Name) as part of the DHCP request.


Resultados 1 - 10 de 99

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.