Consultar las preguntas frecuentes



ACRP1XX, ACRD5XX, ACRP5XX, and ACRC5XX Parts List
... , 5/ 8 IN 7/ 8 OUT R- ... CLASS II 100va 208 - 230 -460- ... C TYRAP 390mm V 0 RATED gt120rv0 ...
EcoBreeze Variable Speed Drive Technical Spec’s
... mA , impedance 800 Ohm , resolution 8 bits AOV configurable voltage 0... 10 V , impedance 470 Ohm , resolution 8 ...
Where can I get support for APC and MGE Products?
... E 47322YL- 8 M-E ... 15F-1 V 51003-6 ... 4 51018- 10 51018-15 ... 6 51019- 10 51019-15 ... 6 51044- 10 51044-15 ...
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
... 2 device from v 5.X.X to v 6.X ... ... Network Management Card v 3.X ... /AP9617/ 8 /9 installed ... Network Management Card v 6.X ... ... 2 device from v 5.X.X to v 6.X ... ... already has BootMonitor v 1.0 ... 8 . Wait for ... ... NMC1 Upgrade Utility v 1.2 ... ... no parity, 8 data bits, ... 8 . Select option ... 10 . Select option ... ... to downgrade from v 6.X.X to v 5.1 ...
Migrate PowerChute Network Shutdown configuration from PowerChute v4.2, v4.3 virtual appliance to v4.4 virtual appliance
... configuration from PowerChute v 4.2, v 4.3 ... appliance to PowerChute v 4.4 ... ... PowerChute Network Shutdown v 4.4 PowerChute v 4.2 ... appliance, PowerChute v 4.3 ... , and PowerChute v 4.4 ... Some v 4.2 ... If your v 4.2 ... ... migrate your PowerChute v 4.2, v 4.3 ... configuration to the v 4.4 ... of the PowerChute v 4.4 ... ... On the PowerChute v 4.2/ v 4.3 ...
NetBotz v3 | How do I configure a PCNS Shutdown alert action?
... action on a v 3 NetBotz Appliance ... NetBotz v 3 (355, 455, 450, 550, & 570) ... NetBotz v 3 (firmware 4.5.4 and higher) ... This feature was not added until NetBotz v 4.5.4. ... 8 ) Check the alert Severities that apply. ... Example: http://10.10.10.10:3052 or https:// 10 .10.10.10:6547 ... 10 ) Click the Advanced ... For more information, see the documentation for PowerChute Network Shutdown v 4.2.
Single Phase Symmetra Drops the Load When Returning from Bypass
Input Voltage: Line I 132.7, Line II 132.7, LI-LII 230 VAC Output Voltage Setting: 208 V ... Output Voltage Setting: 208 V
Hardwiring to 120v, 208v, and 240v loads from a 208v/240v SmartUPS RT UPS
To supply a 208 v load, the transformer provides: 120 v Hot Leg
NetBotz 750 | Physical Description
NetBotz v 5.X ... a maximum of 10 A. Activates ... ... 0-5 V sensors. ... 0-5 V sensors require the ... 0-5 V sensor cable ( ... 8 10 /100/1000 Network Port Provides a connection to the network. ... 9 Private LAN Provides a 10 /100/1000 connection to a private local area network and 48 VDC to an attached device. 10 Wireless Sensor Coordinator USB Port with Wireless NetBotz USB Coordinator (nbwc100u) installed.
What does the Force Negotiation setting achieve in the Network Management Card?
Also, note that the network management card will take the greater of the two values (low battery setting vs . minutes Network Shutdown required shutdown delay). If you set the command line shutdown of 8 minutes on the client but have a low battery of 10 minutes, the card will take the 10 minute value as the max required delay.


Resultados 1 - 10 de 50

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.