Consultar las preguntas frecuentes



Where can I get support for APC and MGE Products?
Service Bypass Panel Service Plans
Why choose glycol over water?
All cooling units that require heat exchangers ... Advantages of Glycol: ... The elimination of corrosion greatly reduces maintenance costs. ... This eliminates the costs of filter maintenance and filtration pump power.
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
... PDU, AV unit , or environmental monitoring unit with an embedded ... ... : Environmental Monitoring Unit 1 (AP9312TH ... ... , Environmental Monitoring Units (ap9320, ... ... firmware to take advantage of enhancements, ... Network Management Cards with the SKU of AP9617, AP9618, or AP9619 use firmware 3.X and Network Management Card 2 units with the SKU of ap9630, AP9631 use version 5.X or 6.X firmware. ... 2. If PowerChute is running, then stop that service . ... 1. Select a serial port at the local computer and disable any service that uses the port.
Smart-UPS SRC 5k, 6k, 8k and 10 KVA FAQ
Q: What are the advantages of the SRC 5-10 KVA LCD Display? ... Q: When do I need to choose a Service Bypass Panel? ... A: In addition to the 1+1 Parallel redundancy system, the Customer can also look into a service bypass panel which will give you a wrap around bypass. ... Q: What are the advantages of the aptf10kw01 Isolation Transformer?
Things To Consider When Upgrading or Downgrading a Network Management Card 2 (NMC2) Device between v5.X.X and v6.X.X
Users wishing to upgrade their firmware (to take advantage of new features and/or bug fixes) ... System name, contact, location, Require DHCP cookie, Telnet, SSH, and CLI settings, Fahrenheit/Celsius display, HTTP server settings, SNMP settings, Data log settings, Event log settings, Syslog settings, Paging settings, Remote Monitoring Service settings, Email settings, and Modbus settings (if applicable)
Problem: PowerChute Network Shutdown does not turn off the UPS following a shutdown event.
Because of this 100-second interval, PowerChute might not have received this information in a couple of situations: a) immediately after installing PowerChute or b) after a restart of the PowerChute service , e.g. after a reboot. To make sure the UPS turns off as planned when a shutdown event occurs, PowerChute shutdown events should be configured with a delay of 120 seconds.
What are the Dynamic Load ratings and Shipping Load ratings for NetShelter CX cabinets?
Persons planning data centers need to know how much weight can be loaded into the NetShelter CX for static installation, dynamic installation (rolling on flat surface) or to ship loaded with equipment. ... These two ratings are different and care should be taken to distinguish between them.
How does the EcoAisle accommodate lighting without interfering with the ceiling panels.
• Many datacenters are planned around the floor tiles, but planning also needs to happen for the illumination of the aisles between the rows of racks. ... There is also a manual switch provided with the system that will allow a user to turn the lights off when exiting the aisle as an extra level of control and energy conservation .
InRow RC Cooling Units installation distances
... install an InRow RC unit it is necessary ... front of the unit and 914mm at ... back of the unit for maintenance and service purposes.


Resultados 1 - 10 de 84

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.