Consultar las preguntas frecuentes



Where can I get support for APC and MGE Products?
Service Bypass Panel Service Plans
Why choose glycol over water?
Advantages of Glycol: ... The elimination of corrosion greatly reduces maintenance costs. ... This eliminates the costs of filter maintenance and filtration pump power. Maximum Heat Transfer
What are the Dynamic Load ratings and Shipping Load ratings for NetShelter CX cabinets?
Persons planning data centers need ... ... Rating is the maximum weight of the ... These two ratings are different and care should be taken to distinguish between them. ... Dynamic Load Weight Rating is the maximum rolling load of the cabinet. This is the maximum allowable weight of equipment installed in the cabinet during movement from one location to another within the same data center. ... Shipping Load Weight Rating is the maximum allowable weight of equipment installed in the cabinet during any shipping process where the cabinet is to be moved outside the data center.
Utilizing the maximum output capacity of the Symmetra RM 6kva
... greater than 5kva, the input to the unit should be hardwired to 40 amp service in order to meet local wiring code requirements.
What are the factors that affect Battery Rated Service Life?
Number of discharges Maximum discharge rate
Smart-UPS SRC 5k, 6k, 8k and 10 KVA FAQ
Q: What are the advantages of the SRC 5-10 KVA LCD Display? ... Q: When do I need to choose a Service Bypass Panel? ... A: In addition to the 1+1 Parallel redundancy system, the Customer can also look into a service bypass panel which will give you a wrap around bypass. ... Q: What are the advantages of the aptf10kw01 Isolation Transformer?
APC Environmental Sensors FAQ
Q. What is the maximum distance the APC Sensors can reach? ... Maximum length of cable - 330 ft ... Maximum length of leak sensing cable - 400 ft ... Maximum length of cable - 330 ft ... Maximum length of cable - 330 ft ... Maximum length of cable - 330 ft ... Maximum length of cable - 330 ft ... Maximum length of cable - 330 ft ... Max length - 1000m ... The door contacts could have any reasonable number of contacts wired within the max cable length above. ... The ap9520t and TH probes have the following advantages :
Problem: PowerChute Network Shutdown does not turn off the UPS following a shutdown event.
Because of this 100-second interval, PowerChute might not have received this information in a couple of situations: a) immediately after installing PowerChute or b) after a restart of the PowerChute service , e.g. after a reboot. To make sure the UPS turns off as planned when a shutdown event occurs, PowerChute shutdown events should be configured with a delay of 120 seconds.
Things To Consider When Upgrading or Downgrading a Network Management Card 2 (NMC2) Device between v5.X.X and v6.X.X
Users wishing to upgrade their firmware (to take advantage of new features and/or bug fixes) ... System name, contact, location, Require DHCP cookie, Telnet, SSH, and CLI settings, Fahrenheit/Celsius display, HTTP server settings, SNMP settings, Data log settings, Event log settings, Syslog settings, Paging settings, Remote Monitoring Service settings, Email settings, and Modbus settings (if applicable)


Resultados 1 - 10 de 95

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.