Consultar las preguntas frecuentes



Can AR7715 or AR7725 be Used with Other Side Airflow equipment?
... be similar to the Cisco models with similar chassis dimensions: 14U x 17.3" W x 24 " D. Installing equipment ...
Video: How can I download Event, Data, Configuration, and Debug files from my Network Management Card?
To begin , here is a list of what ... ... v3. X . X , v5. X . X , and v6. X . X firmware versions. Open a command prompt (In a Windows environment: Start > run > ... If using a GUI FTP client ... ... , files are now stored in the ... ... The files have now been downloaded and ... ... (ap9640/ 41 ) - How ... ... technical support, a single debug file ... ... Management Card via a supported web browser ... ... .) Choose a location on your ...
PowerChute Network Shutdown - Shutdown Procedure for VMware vSAN with vSphere 7.x
... When carrying out a cluster-wide ... , there is a risk that some ... become unavailable if a failure occurs during a cluster start up.
How do I upgrade and activate premium devices in StruxureOn?
... .4. X When you start using the StruxureOn ... To upgrade a device About Premium 24 /7 expert ... ... devices 24 hours a day, 7 days a week enabling remote ... ... Electric experts for a quick resolution of a problem. Proactive service dispatch To upgrade a device ... of devices select a device you want ... This is a Premium device. The first time you upgrade ... , a number icon will appear on Settings>Premium ... Once you have completed the upgrade process, Premium features will be available immediately and you will see an icon next to your device indicating that this is now a Premium device.
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
You have a device such as a Rack PDU, ... You had a problem with a previous upgrade attempt ... ... Also, sometimes a firmware upgrade can ... ... v5. X . X to v6. X . X , please review ... Begin by determining what ... ... multiple devices at a time, ... AP9635 installed in a Symmetra PX 250 ... , you have a Network Management Card ... ... Card installed in a UPS, you ... ... if you have a Smart UPS 750 ... ... v3. X . X Firmware for Smart ... ... v6. X . X Firmware for Smart ...
Mass Configuration of Users and User Preferences on Network Management Card 2 (NMC2) v6.X.X
... will have the same preferences (which are now configurable on a per-user basis), you can modify these settings first so ...
EcoBreeze Variable Speed Drive Technical Spec’s
Line current 71.9 A for 240 V 82.1 A for 200 V ... ... 28.5 kVA Maximum transient current 99 A for 60 s ... V ≤ 100 A for overload and ... ... V ≤ 10 A for overload and ... Continuous output current 66 A at 4 kHz Transient overtorque 150 ... ... ... braking resistor continuously 150 % without braking resistor ≤ 150 % with braking ... ... Ohm AI3 configurable current 0.. ... ... type AOC configurable current 0.. ... Minimum switching current R1- ...
PowerChute Business Edition version 9.1.x, v9.5 Agent - Potential Issues with Overlapping Scheduled Shutdowns
It is advisable not to schedule overlapping schedules with a higher priority schedule starting first if you have a UPS with both a MOG and ...
Why am I receiving a "serial communication lost" message from my Network Management Card?
All serial numbers Older firmware revisions beginning with v1. X , 2. X and 3. X


Resultados 1 - 10 de 95

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.