Consultar las preguntas frecuentes



Can you hardwire the input/output of the Matrix-UPS?
Input Over-current Protection 3kva: 20 A
What are the basic troubleshooting steps for the Universal Transfer Switch model UTS6H?
A 20 A fuse is installed ... the use of a 15 A fuse. Remove ... the existing fuse with a fuse of correct amperage.
What are the basic troubleshooting steps for the Universal Transfer Switch model uts10bi?
A 20 A fuse is installed ... the use of a 15 A fuse. Remove ... the existing fuse with a fuse of correct amperage.
What are the basic troubleshooting steps for the Universal Transfer Switch model UTS6 / UTS6BI?
A 20 A fuse is installed ... the use of a 15 A fuse. Remove ... the existing fuse with a fuse of correct amperage.
Hardwiring to 120v, 208v, and 240v loads from a 208v/240v SmartUPS RT UPS
This creates a traditional 240 v/ 120 v panel where there ... 2 legs of 120 v and from hot ... would measure 240 volts .
How do I update the firmware of my SRT, SMC, XU, XP, SMX, SMT, SMTL, SCL, SRC, CHS series Smart-UPS?
Devices that do *NOT* have upgradable firmware: These units are 120 V devices built prior to date code 1037. Date code is the first 4 numbers in your serial number.
How do I update the firmware of my SRT/SMC/XU/XP/SMX/SMT/SCL/SRC/CHS series Smart-UPS using the Firmware Upgrade Wizard?
Issue: These units are 120 V devices built prior to date code 1037. Date code is the first 4 numbers in your serial number.
What are the basic troubleshooting steps for the Smart-UPS smx1500rm2u ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smx2000hv / smx3000hv ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smx2000lv / smx3000lv ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)


Resultados 1 - 10 de 68

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.