Consultar las preguntas frecuentes



Battery Discharge During Storage
At 20° Celsius, a battery will lose 3% of its capacity per month .
SmartConnect Portal indicates that the firmware is out of date on my SmartConnect enabled UPS. How do I update it?
... SmartConnect enabled ( EcoStruxure ™ Ready) ... EcoStruxure ™ Ready Smart ... EcoStruxure ™ Ready Smart-UPS products are able to download the latest UPS Firmware from the Cloud. ... https://www.smartconnect- support .apc.com/help/EN/index.html#page/ EcoStruxure %2520ready%2520smart-UPS%2520help%2520center%2fmn04.6.2.html%23 ... 1 - To upgrade the firmware you can do so via the cloud portal.
Data Center Expert | What virtualization environments are supported?
... virtualization environments are supported for the Data ... ... recent information on supported virtualization platforms can ... found within the EcoStruxure IT Help Center at ... ... virtual appliance, supported on VMware ESXi ... ... device nodes and one surveillance node. ... nodes and activate supported applications, or ... ... is the first supported virtualization platform. The Data Center Expert virtual appliance is delivered as an OVA (Open Virtualization Archive), expected to function properly on any virtualization platform that supports this format, or has an appropriate converter utility. ... There is currently no planned support for any other virtualization platforms, including Microsoft Hyper-V.
Configuring the Native Serial Shutdown Support in Windows 2000, XP, or 2003
How to Configuring the Native Serial Shutdown Support in Windows 2000, XP, or 2003 ... Native serial shutdown is not supported with Smart-UPS model family SMT, SMX, ... Step # 1 : ... Note 1 : ... 1 Stop Bit ... UPS, you will also receive information such as Runtime, Battery Capacity and battery condition. ... If hibernation is not enabled, there will be no hibernation tab and it will not be listed in shutdown ... If this is the case, your BIOS may not support hibernation or it may be disabled.
NetBotz 300-500 Series | Downloading and Installing the Advanced View Management Software
... NetBotz 300- 500 Series [v ... ... NetBotz 300- 500 Series [v ... 420, & 500 ) ... NetBotz 300- 500 series appliances can ... It is recommended that ... 1 ) Navigate to ... ... of this if it is not needed ... ... , 420, 500 Products that require the use of Advanced View 2.6 is End-of-Life and End-of- Support . It is highly recommended to look at purchasing newer appliances. ... 1 ) Download the Advanced View 2.6 Installer File from BOX: ... You can exit out of this if it is not needed.
kvm0216a KVM Series Bus Communication Behavior
It also supports ( 1 ) or (2) bus cascading.
Data Center Expert | Discovering a NetBotz 300-500 Series Appliance
... 400, or 500 series appliance into ... ... (nbrk0450/ 1 ), 550 ... ... NetBotz 300- 500 Series Appliance ( ... ... is currently not supported ... NetBotz 300- 500 Series Appliance 1 ) Log into ... It is recommended to ... ... NetBotz 300- 500 & 700 series ... It is not recommended ... of system resources it takes to run ... ... /time within it . ... Appliance 300- 500 Series Device Discovery ... ... NetBotz 300- 500 Series Discovery 1 ) Log into ... Your network team should be able to tell you if ICMP traffic is blocked on the network, but on most networks it is available for use. ... Discovering a NetBotz 300- 500 Series Appliance
Where can I get support for APC and MGE Products?
... 6 0034- 1 0034-100 ... 2M- 1 E 0035nd-3M- 1 E 0039- ... ... 2M- 1 E 0088nd-3M- 1 E 0100- ... 2M- 1 E 0226- ... 3 0377- 1 M 0377- ... ... 2M- 1 E 0719- ... 7 0859- 1 0859-10 ... ... 15M 12000- 1 M 12000- ... 15M 12008- 1 M 12008- ... 15M 12012- 1 M-E ...
Data Center Expert | How do hardware and software support contracts work?
... warranty and software support contracts work for ... Software Support Contract software support . ... and complete software support in order to receive technical support and software upgrades ... Software support contracts are required ... under base software support SKUs) as ... ... not currently require support contracts. Hardware Support Contracts Hardware support must be continuous ... Year 1 ... Out of HW Support ap9470 Factory Factory ... Out of HW Support AP9475 Factory Factory ... Out of HW Support Software Support Contracts Software support can not be ... virtual appliance until it is activated using ... Support contracts start at ... ... systems, the support will begin when ...
Why is my Web/SNMP (ap9606) or Network Management Card 1, 2 or 3 not recognizing my UPS or device?
... Card in a supported UPS or device ... try to access it through either the ... ... Environmental Monitoring Unit 1 (AP9312TH) ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... ... firmware application on it . Single or three phase ... Single phase Smart- ... Single Phase Symmetra UPS ... PX 250/ 500 ... Management Cards, it may be a ... Try a different Network Management Card in the original UPS (verifying its firmware is also up to date and correct). Trying the original Network Management Card in a different UPS (verifying its firmware is also up to date and correct). ... APC Technical Support


Resultados 1 - 10 de 92

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.