Consultar las preguntas frecuentes



Data Center Expert | Trial version VM appears to have 25 nodes available.
... Machine or VM version shows this same 25 node license key in the user interface however until activated, will only allow 5 nodes to ...
Data Center Expert | How do hardware and software support contracts work?
... for StruxureWare Data Center Expert . StruxureWare Data Center Expert (DCE) StruxureWare Data Center Expert (all versions ... StruxureWare Data Center Expert appliances come with ... The Data Center Expert appliance and any ... ... a default 25 nodes (covered under ... as each additional node license . Modbus license keys and surveillance keys do not currently ... StruxureWare Data Center Expert Appliances can have ... a total of 5 years, which ... Year 5 ... virtual machine activation key (AP94VMACT) ... ... your server and license keys back under support ... ... amount of Device Nodes Installed ... number of install licenses .
Data Center Expert | What virtualization environments are supported?
... for the Data Center Expert virtual appliance? StruxureWare Data Center Expert (DCE) StruxureWare Data Center Expert (all verisons ... ... EcoStruxure IT Help Center at: ... -Data- Center - Expert -Virtual- ... The Data Center Expert v7. ... ... monitors up to five device nodes and one surveillance node . ... can purchase a license key to upgrade to ... monitor additional device nodes and activate supported ... ... of the Data Center Expert 7.2 ... The Data Center Expert virtual appliance is delivered as an OVA (Open Virtualization Archive), expected to function properly on ...
Data Center Expert | Why does StruxureWare not accept my One Time passcode?
StruxureWare Data Center Expert is not accepting ... StruxureWare Data Center Expert (DCE) ... StruxureWare Data Center Expert (all versions ... SturuxureWare Data Center Expert requires a 64 character license key that is created ... and the Data Center Expert's MAC address. StruxureWare Data Center Expert (DCE) ... ... when purchasing a license key is not the actual license . ... passcode to a license key . 5 . To add ... ... = StruxureWare Data Center Expert Basic ... = StruxureWare Data Center Expert Standard ... = StruxureWare Data Center Expert Enterprise ... = StruxureWare Data Center Expert Virtual Machine ... = StruxureWare Data Center Operation
Data Center Expert | Migrating from a Physical Appliance to a Virtual Appliance
StruxureWare Data Center Expert (DCE) StruxureWare Data Center Expert (all versions ... ... As the data center is moving away ... ... the AP94VMACT activation key to activate the ... ... server already has licensing on it ( ... base 25 device nodes and 1 surveillance node ) your will ... License keys are tied to ... ... contracts for the license keys and the server ... can reset the license key passcodes so that ... used again to license the virtual server ... ... new servers/ licenses . 5 ) During deployment ... ... support for the license keys against this mac ... ... redeem the activation key passcode as well ...
Data Center Expert | Getting Started
... with a Data Center Expert Appliance. StruxureWare Data Center Expert (DCE) StruxureWare Data Center Expert (all versions ... ... the Physical Data Center Expert Appliance ... the Virtual Data Center Expert Appliance ... is restricted to 5 nodes . ... you have purchased licensing , continue to ... the passcodes for licenses . ... the StruxureWare Data Center Expert Virtual Appliance? ... storage that Data Center Expert has within VMWare ... Getting Data Center Expert on the Network ... that your Data Center Expert (DCE) ... ... for StruxureWare Data Center Expert StruxureWare Data Center Expert Security Information ( ... Licensing and Software Support
Can I transfer license keys between StruxureWare Data Center Expert servers?
Product Line: StruxureWare Data Center Expert (DCE)
Video: Data Center Expert | How do I enable surveillance for NetBotz cameras?
You can verify the licensing that you have installed by going to: System Menu > Server Administration Settings > License Keys .
Video: How do I register a passcode for NetBotz or StruxureWare?
... Depending on what type of license key you are redeeming ... either: Data Center Expert Model, NetBotz ... SFDCOBase (Data Center Operation).
Video: Data Center Expert | Desktop Client Requirements, Download, & Installation
... the StruxureWare Data Center Expert desktop client software ... Struxureware Data Center Expert (DCE) Struxureware Data Center Expert (all versions ... ... for the Data Center Expert software. ... deploying the Data Center Expert Virtual Appliance on ... ... The StruxureWare Data Center Expert Desktop Client ( ... ... Agree to the license agreement. 5 ) Run the downloaded execuatble file and follow the on-screen instructions. 6) Once the installation completes, you can launch to the Desktop Client using the Desktop Icon (if done during installation) or the Start Menu Option for StruxureWare Data Center Expert #.#.#.


Resultados 1 - 10 de 64

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.