Consultar las preguntas frecuentes



Did APC purchase the AirFlow Company?
Did APC purchase the AirFlow ... APC purchased Airflow in ... Air Division under APC . American Power Conversion Expands Availability Solutions with Acquisition of Airflow Company ... will operate within APC’s Availability Enhancements Group, further strengthens APC’s stature as a ... ... Jr., APC’s president and CEO ... ... The marriage of APC and Airflow is ... win, providing APC with entry into ... business while leveraging APC’s global scale, ... ... to industry and APC estimates, Airflow ... ... A precision cooling device goes beyond commercial ... ... additional equipment to manage humidity levels. ... Since 1997, APC has made a ... ... to standardize on APC for virtually all ... ... customer segments, APC is the ideal ...
Why can't I connect to my APC Network Management Card or embedded Network Management Card using a serial connection?
by the user, a change to the configuration file, or a managing device like ISX Manager or StruxureWare Central.
Why doesn't StruxureWare or ISX Manager's mass configuration feature update or show password credentials on APC Network Management Card devices?
... Mass configurations of APC UPS Network Management ... Management Card enabled devices done via ISX ... version of the devices . Devices with an embedded ... Devices with an embedded ... Devices with an embedded ... ... , or any devices with an integrated ... ... , or any devices with an integrated ... ... passwords specifically are managed completely outside of ... ... make mass configuration change of the various ... Manager takes one device's configuration file and ... them to other devices . ... new passwords to devices , just not ... one from another device . ; To change the Administrator, Device , or Read ... ... , AdminPassword= apc
Video: Data Center Expert | Managing Users
Managing Users within StruxureWare ... Managing Local Users ... select Users and Device Group Access ... only the local apc user. ... that may help manage permissions for multiple ... ... select Users and Device Group Access ... select Users and Device Group Access ... to save the changes . ... select Users and Device Group Access ... select Users and Device Group Access ... 2) Click Device Group Access ... once) a device group in the ... ... ) Click Modify Device Group Access ... to save the changes . Managing Remote Users ... be used to change the password for ... ... select Users and Device Group Access
Video: Why might my APC Back-UPS Product be beeping?
APC's UPS Selector ... unit shipped with APC management software it ... be possible to change the default acceptable ... ... section of the APC management software for ... ... no way to change the +/ ... ... the ability to change their sensitivity to ... ... automatically if the APC management software is ... contact APC Support APC's UPS Selector. APC recommends plugging only ... contact APC Support ... to a new APC Back-UPS ... Managing UPS Audible Alarm ... via On- Device Mute Feature ( ... ... Quick Mute on APC Back-UPS ... ... Audible Alarms on APC Back-UPS ... Managing UPS Audible Alarm ... Once the computer has detected the "New Hardware Device ", onto a currently supported operating system.
How To: Configuring an APC Network Management Card with popular email services such as Gmail, Yahoo!, Office 365, and Hotmail/Outlook.com
... working with an APC Network Management Card-enabled device or need to ... Devices with an embedded ... Devices with an embedded ... Devices with an embedded ... ... Network Management Card device send email to ... ... is recommended you change the From Address ... that TCP port 25 is open. ... ISP's block port 25 since it has ... ... mail server, changing your From Address ... , and NMC3 devices ... is recommended you change the From Address ... ON for your APC NMC device to be allowed ... ... email test after changing it. If this does not work, please ensure that port 25 is open ( ...
Creating an Aggregate Device within the KVM Access Software
... create an aggregate device within the KVM ... Aggregate devices can be created when a device (router, ... .,) managed through KVM Access ... accessed through several devices ’ ports. ... a single Aggregate Device , the Aggregate Device counts as a ... requires a single license . ... creating an aggregate device allows the end ... end user to manage power to that ... ... behind the aggregate device is to allow ... user to tie devices together to make ... that specific aggregate device , shut down ... ... have 300 node license but have 300 ... 900 total target devices , (servers ...
Data Center Expert | Using APC SNMP Device Configuration to change SNMP settings may disassociate the current notification policy for that device.
Cause Switching the protocol used for communication between Data Center Expert and APC Devices from snmpv1 to snmpv3 may disassociate the current notification policy.
MAC address Vendor ID of Network Management Cards, and other network devices changing
The APC Device IP configuration wizard uses the MAC address to identify unconfigured APC network cards.
Video: Data Center Expert | How do I create and manage thresholds?
APC devices have device alerts by default, but can still have additional thresholds created for them within DCE.


Resultados 1 - 10 de 83

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.