Consultar las preguntas frecuentes



Video: How do I upgrade my Smart-UPS firmware using my Network Management Card?
... are the steps in order to use my Network Management Card 2 or 3 to update my Smart ... ... , AP9631, or AP9631CH) with ... 6.4 or higher ... Correct firmware file for the particular UPS ... ... Firmware Updates allow for continuous improvements and ... ... the APC Firmware Upgrade Wizard via a Serial or USB connection to the UPS whenever ... ... The APC Firmware Upgrade Wizard guides you through the upgrade process and incorporates ... a more consistent upgrade experience. ... find the Firmware Upgrade Wizard in Kbase # .
How do I perform a mass firmware upgrade on APC network enabled products?
... a mass firmware upgrade on APC network ... ... How can I upgrade firmware on multiple ... at one time or in an automated fashion ... ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but are not limited to ): Metered ... , Environmental Monitoring Units (ap9320, ... ... are not limited to ): 2 ... ... user may wish to automate the process of upgrading firmware on Network Management Cards or devices with an embedded card to save time, ... Users can upgrade the firmware on ... Firmware Upgrade Utility (the ...
What are the typical uses for an EcoAisle System
... the typical uses for an EcoAisle System ... ... solutions are designed for close temperature control ... ... provide high reliability for year-round ... and redundancy necessary to keep the technology room up and running ... ... conditions is critical to smooth operation of ... ... essential because fluctuations in the temperature of ... and premature failure in IT equipment. ... the inlet temperatures to the equipment will ... constant and adequate for proper operation. ... cooling problems arise in the data center ... ... The EcoAisle allows for more predictable cooling in this new IT ... and cold airstreams in the IT Environment ... ... streams are channeled to their required locations ...
Why isn’t snmpv3 working properly in Network Management Card AOS versions 3.5.7 and earlier?
... 5.7 or below). ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but are not limited to ): Metered ... , Environmental Monitoring Units (ap9320, ... In some cases, ... may find that one more of the ... “timeout” or have communication issues ... Network Management Card 1 (AP9617, ... ). In such cases, ... resetting the card to defaults fixes this ... ... the firmware fix for this issue. ... Please seek an upgrade if you are ...
UPDATED MARCH-2016: Unable to access my APC Network Management Card (NMC) enabled device via HTTPS (SSL/TLS)
... user is unable to access their APC ... ... are two parts to this issue, ... Card product configured for SSL (HTTPS ... ... sslv3.0 in their browser products due to numerous security vulnerabilities ... One such vulnerability is ... ... will fall back to sslv3.0 ... , be vulnerable to POODLE. ... ) is configured for HTTPS. ... ) is configured for HTTPS. ... Card is configured for HTTPS. ... _key, or anything referring to invalid key size ... may be due to a separate issue entirely or an additional issue ... ... Network Management Card 1 (NMC1) ...
APC UPS Network Management Card (NMC) Compatibility Chart
... Card is supported in my UPS? ... Network Management Card 1 - AP9617, ... ... has been created for reference. Please refer to the table below ... ... cards, support for new device features or management card features ... Network Management Card for your device. ... application file, for use with the ... Firmware files for use in other UPS systems ... choose "Firmware Upgrade ") Single and Three Phase ... ... Symmetra LX ( Single phase Symmetra UPS ... ... , supported added for some SmartUPS 3 ... ... Phase Galaxy UPS units : ... Includes built- in network management card ...
Rack PDU 2G (AP8XXX) Network Port Sharing Information
... .6 rpdu2g or higher (except ... Users interested in Network Port Sharing ... giving the ability to share one IP address via one network connection) Refer to the detailed information ... ... Port Sharing feature to view the status ... and manage up to four Rack PDUs using only one ... via the " In " and " ... ... All Rack PDUs in the group must ... , 5. 1 .6 or later (excluding ... EnergyWise), in order to support the Network ... ... a number, 1 to 4, used to uniquely identify the Rack PDUs in a group.
How to set up group communications for an Network Air FM unit
... instructions on how to set up group communications in a Network Air FM unit . ... this document is to provide a clear communication on how to properly configure a group of FM units to work together. ... Redundant Group Control or RGC is a ... two, three or four systems that ... In order to better understand RGC, we need to define the different ... ... independent, Computer Room Air Conditioner. ... a set of one to three Modules operating ... all the modules in that system.
INFORMATION BULLETIN: Important information regarding firmware upgrade to rpdu 3.5.7 or rpdu 3.5.8 firmware revisions
... Rack power distribution units (AP79XX only ... warned that when upgrading from an earlier ... of PDU firmware to 3.5.7 or 3.5 ... Update 1 /30/ ... ... 7.0 or higher which addresses ... ... an earlier revision to 3.7.0 or higher will keep ... ... new firmware from or through ISX Manager ... Users upgrading to rpdu v3 ... 5.7 or v3. ... ... Rack power distribution units (AP79XX only ... warned that when upgrading from an earlier ... of PDU firmware to 3.5.7 or 3.5 ...
Can I plug my APC Rack-Mount Power Distribution Unit (Rack PDU) into a feed receptacle located in the under floor plenum? (Also applicable to Configurable & Modular Power Distribution)
... the installation conforms to NFPA 70 the ... requirements as stated in Article 645 Information ... Refer to the complete section ... of the NEC for your locality. 645.5 Supply Circuits and Interconnecting Cables ... shall be permitted to be connected to a branch circuit ... ( 1 ) Flexible cord ... plug cap not to exceed 4. ... ( 1 ) The raised ... ... circuit supply conductors to receptacles or field-wired equipment are in rigid metal conduit ... metal conduit, or liquidtight flexible nonmetallic ... ... MC cable, or Type AC cable ... ... shall be installed in accordance with the ... ... information technology equipment in accordance with 645 ...


Resultados 1 - 10 de 83

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.