Cable Picture Degradation When Using an APC Coaxial Surge Protector
... After connecting an APC device with Coax Protection , customer observes ... SurgeArrest , Protectnet, Back-UPS, Back-UPS Pro, APC AV line of products ... Most television tuners require 7 dB ... them, then 7 dB is all that is left for both. ... connected which requires 4 dB, the chances of 'ghosting' or lines being present ... Inserting a cable protector like an APC ... APC Coax protection has been tested from 30 MHz to 1 GHz. ... terminated cables from an electronics store ; such as Radio Shack. ... (available at many electronics stores ).