Browse FAQs
NetBotz 250 | Network Port Light Indicators
Published date:
04 September 2019
Browse FAQs
Condition | Description |
Off | One or more of the following situations exist:
|
Solid Green | The Rack Monitor 250 is connected to a network operating at 10 Megabits per second (Mbps). |
Solid Orange | The Rack Monitor 250 is connected to a network operating at 100 Mbps. |
Flashing Green | The Rack Monitor 250 is receiving or transmitting data packets at 10 Mbps. |
Flashing Orange | The Rack Monitor 250 is receicing or transmitting data packets at 100 Mbps. |
Condition | Description |
Off | One of the following situations exists:
|
Solid Green | The Rack Monitor 250 has valid TCP/IP settings. |
Flashing Green | The Rack Monitor 250 does not have valid TCP/IP settings.1 |
Flashing Orange | The Rack Monitor 250 is making BOOTP requests. |
Rapidly Flashing Green | A user initated a LED blink test from the user interface. |
Alternately flashing green and orange | If the LED is flashing slowly, the Rack Monitor 250 is making DHCP requests.1 If the LED is flashing rapidly, the Rack Monitor 250 is starting up. |