Browse FAQs

How to create a local user account that PowerChute will use to communicate with VMware ESXi hosts and vCenter Server Appliance.

Published date: 22 October 2020

Issue:
Need to create a local account the PowerChute will use to communicate with VMware ESXi hosts and vCenter Server Appliance.

Product:
PowerChute Network Shutdown v4.2, v4.3, v4.4

Environment:
VMware ESXi 6.7, 7.0 
VMware vCenter Server Appliance 6.7, 7.0

Cause:
Informational

Solution:
Please view the attached videos

NOTE: For assistance with creating local account on vCenter Server that is running on Windows OS see Schneider Electric FAQ FA241010
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.