Browse FAQs

What is the maximum mounting depth of a 1070mm (42") deep NetShelter SX cabinet with no accessory mounting rails?

Published date: 15 May 2019

Issue:
A customer needs to know the maximum available mounting depth. 

Product Line:
NetShelter SX 1070mm Deep

Environment:
All versions and serial ranges.

Cause:
A customer has very deep equipment and wants to know if it will fit into the cabinet. 

Resolution:

The maximum spacing for an AR3100 is 35.75”. At this spacing, the rear accessory/PDU mounting rails must be removed. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.