What are the condenser pressure drop and temperature limitations on the ACSC?
Published date:
11 June 2020
Issue:
What are the condenser pressure drop and temperature limitations?
Product line:
ACSC100, ACSC101
Environment:
InRow Cooling Cause:
Resolution:
It is recommended that you have no more than 0.25” (65 Pa) of additional external pressure drop. The condenser should see inlet temperatures of 32-105 F (0-40 C), 70-86 (21-30 C) in ideal conditions. See Application Note #109 for further details.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.