Browse FAQs
Can I operate my A/C in ambient temperatures below 65f
Published date:
13 February 2014
Browse FAQs
Issue:
Can I operate my ac in ambient temperatures below 65f
Product line:
All compressor ac units
Environment:
All Product models, all serial numbers
Cause:
Condition called flood back
Resolution:
Recommendations for operating at lower ambient conditions
If you are going to be operating the system below 65F, you should add the items below.
1) there should be a crankcase heater installed on the compressor
2) a low ambient control
3) suction line accumulator
4) confirm compressor superheat
These items will assist in preventing liquid floodback, flooded starts, and refrigeration migration during off cycle. These situations are detrimental to the life of the compressor.