Browse FAQs
Can I extend the length of my Environmental Sensors and Probes?
Published date:
04 June 2019
Browse FAQs
Issue
Can I extend the length of my Environmental Sensors and Probes?
Product Line
Cause
This document pertains to the Environmental Sensors and Probes that can be connected to APC's Environmental Monitoring and Management Units (AP9312, AP9319, AP9320, and AP9340) and version 3 NetBotz Appliances.
Resolution
Additional information on connecting Environmental Sensors and Probes can be obtained via the User's Manual for the AP9312, AP9319, AP9320, AP9340, and current NetBotz products.