Consulter la FAQ



Modbus Installation and Troubleshooting for AP9635/AP9635CH Network Management Card 2 (NMC2)
... Modbus TCP or Modbus RTU with AP9635/AP9635CH ( Galaxy VM, Galaxy 300/7000, Galaxy 5000 / 5500 , etc)
Galaxy 5000; Modbus Q1 Input Breaker status does not change state
Modbus Q 1 Input Breaker status ... NAM Galaxy 5000 NAM Galaxy 5000 Modbus Q 1 Input Breaker status ... Resolution : ... The 66061 JBUS/Modbus manual was updated May 2018 to reflect the correct Modbus register for NAM Galaxy 5000 Q 1 Breaker status. The Q 1 Modbus register is only monitored on EMEA Galaxy 5000 / 5500 UPSs. For NAM Galaxy 5000 customer must monitor KA1 for Q 1 Breaker status change. ... Status to 1 ... 1 input switch (Q 1 ) in EMEA ... 1 backfeed (KA1 optional) ... Status to 1 ... 1 input switch (Q 1 ) in EMEA ... 1 backfeed (KA1 optional)
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel. ... Galaxy 5000 , Galaxy 5500 ... Due to site maintenance, inclement weather, and other conditions, request come in for assistance with Powering Down the Galaxy 5000 UPS Resolution : ... This procedure is for a single UPS with an external maintenance bypass panel. ... Step 1 : Touch any button on the display to wake it up. ... Turn off Q 1 Switch
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
Shutting Down the MGE Galaxy 5000 UPS ... Galaxy 5000 , Galaxy 5500 ... Due to site maintenance, inclement weather, and other conditions, request come in for assistance with Powering Down the Galaxy 5000 UPS Resolution : ... This procedure is for a single UPS without an external bypass panel. ... Step 1 : Touch any button on the display to wake it up. ... Step 6: Turn the Q 1 Switch to Off
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Transitioning the Galaxy 5000 UPS from total power off to normal on-line operation. ... Galaxy 5000 , Galaxy 5500 ... For various reasons, the Galaxy 5000 may be in a totally off state. ... Resolution : ... How to restore the Galaxy 5000 UPS from total power off to normal operation. This procedure is for a single UPS without an external bypass panel. ... Step 1 : Set the input Q 1 switch to On
MGE Galaxy 5000 Installation, Technical Specs and Operation Manuals
... com/shop/us/en/products/MGE- Galaxy - 5000 -100- kVA /P-g5tups100
Galaxy 5000, Galaxy 5500; Dust Covers
MGE Galaxy 5000 , Galaxy 5500 , Dust Cover, Input Wiring, Installation , foreign conductive particles,
Video: How to determine which firmware to install on the 66074 NMC is by the color of the PCB
Galaxy 5000 / 5500 , Upsilon/ ... , eps8000, Galaxy 4000, Galaxy 3000, Galaxy PW, Comet ... which firmware to install on the 66074 ...
Information for Colors of UPS Galaxy 5000, Galaxy 5500
Due to dent and paint scratch or marks customer needs information about colors used. Resolution :
​Information for Noise level of UPS Galaxy 5000 NAM
Information for Noise level of UPS Galaxy 5000 NAM ... Galaxy 5000 NAM ... Galaxy 5000 40kva, 50kva,60kva, 80kva, 100kva and 130kva ... Customer needs UPS room noise level with Galaxy 5000 . Resolution : ... for Galaxy 5000 . ... UPS rating ( kVA ) 40/50/60/80kva 100/130kva Noise level on a normal floor (dBA) with an RL load at 3 feet 65 63


Résultats 1 - 10 de 61

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.