Consulter la FAQ



How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
... to take the Single Galaxy 5000 UPS from ... Galaxy 5000, Galaxy 5500 ... Powering Down the Galaxy 5000 UPS Resolution : ... This procedure is for a single UPS with an external maintenance bypass panel. ... Step 1 : Touch any button on the display to wake it up. ... Step 5: Press the Inverter OFF (gray) button for 3 seconds to transfer the load to the Static Bypass Switch . At this point, the load is no longer protected by the UPS. ... Turn off Q 1 Switch Turn off Q4S switch
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
... Down the MGE Galaxy 5000 UPS Galaxy 5000, Galaxy 5500 ... Powering Down the Galaxy 5000 UPS Resolution : ... is for a single UPS without an ... Step 1 : Touch any ... Step 5: Press the Inverter OFF (gray) button for 3 seconds to transfer the load to the Static Bypass Switch . At this point, the load is no longer protected by the UPS. Step 6: Turn the maintenance bypass switch Q3BP to ON. Step 4: Turn the output switch Q5N to OFF. ... Step 6: Turn the Q 1 Switch to Off Step 7: Turn the Q4S Switch to Off
Smart-UPS VT and Galaxy 3500 Power Off, Bypass and Power on Procedures
... UPS VT and Galaxy 3500 Power Off ... ... Ups VT, Galaxy 3500 ... Ups VT and Galaxy 3500 Power off ... Resolution : ... all the batteries by sliding out about ... ... with UPS in static bypass. Turn Q 1 to OFF position ... Disconnect all the batteries by sliding out about an inch so they are not making contact with the UPS. ... Turn ON Q 1 (wait about 30 seconds.) ... Switch Q2 to ON. Q 1 , Q2 and Q3 should all be ON at this stage UPS in bypass and in Maintenance bypass (Q3 closed)
Which SmartSlot accessories are supported by the Galaxy 3500 (g3500) UPS?
... accessories are supported by the Galaxy 3500 (g3500 ... MGE Galaxy 3500 models ... accessories are supported by the Galaxy 3500 UPS ( ... Resolution ... inputs, ( 1 ) output per ... ... AP9613 utilizing dip switch configurations only) ... 1 .) Purchase ... ... an APC ap9600 single slot SmartSlot expansion ... ... is the proper installation order per . ... This required installation order also applies ... ... referencing the correct installation order mentioned in The Interface Expander 2 (AP9624) is also supposed by the g3500 and was released in mid-2014 to replace ap9607 and ap9607cb.
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Transitioning the Galaxy 5000 UPS from ... Galaxy 5000, Galaxy 5500 ... reasons, the Galaxy 5000 may be ... The commissioning of a new UPS must be performed by a Schneider Electric trained and qualified service representative. Resolution : ... How to restore the Galaxy 5000 UPS from total power off to normal operation. This procedure is for a single UPS without an external bypass panel. ... Step 1 : Set the input Q 1 switch to On ... Step 5: Turn the Q4S Switch to On Step 6: Turn the output switch Q5N to On Step 7: Turn the maintenance bypass switch Q3BP to Off
Smart-UPS VT-Galaxy 3500; Bypass Not Available Input Freq/Volt Out Of Range, Output: Inverter sync. to bypass alarms
... UPS VT- Galaxy 3500; Bypass ... ... UPS VT- Galaxy 3500-ais3000 ... and indicates that static Bypass operation may ... ... you to enter Static Bypass operation, ... 60 HZ +/- 0, 1 % ... 50 HZ +/- 0, 1 % ... Resolution : When AC mains returns you may get a informational event for; Mains no longer prevents UPS from switching to bypass.
Galaxy 5000; Modbus Q1 Input Breaker status does not change state
Modbus Q 1 Input Breaker status ... NAM Galaxy 5000 NAM Galaxy 5000 Modbus Q 1 Input Breaker status ... Resolution : ... The 66061 JBUS/Modbus manual was updated May 2018 to reflect the correct Modbus register for NAM Galaxy 5000 Q 1 Breaker status. The Q 1 Modbus register is only monitored on EMEA Galaxy 5000/5500 UPSs. For NAM Galaxy 5000 customer must monitor KA1 for Q 1 Breaker status change. ... Status to 1 ... 1 input switch (Q 1 ) in EMEA ... 1 backfeed (KA1 optional) ... Status to 1 ... 1 input switch (Q 1 ) in EMEA ... 1 backfeed (KA1 optional)
Modbus Installation and Troubleshooting for AP9635/AP9635CH Network Management Card 2 (NMC2)
... support Modbus TCP or Modbus RTU with AP9635/AP9635CH ( Galaxy VM, Galaxy 300/ 7000 , Galaxy 5000/5500, etc ...
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
... all products supported by 66061 – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... all products supported by 66061 – STS, Galaxy 3000, 4000, 5000 and Galaxy PW Resolution : ... The 66061 JBUS/Modbus card is configured for 9600, 8, N and 1 . Slave address is 1 and wiring is 2-wire with no parity and termination. This assumes only one 66061 card or UPS or STS is connected to the enclosure but if more than one change as required. ... One is down (off position) and all others are up.
Galaxy 3500, Smart-UPS VT and ais3000 Power Factor Information
Galaxy 3500, Smart-UPS VT and ais3000 Power Factor Information ... Galaxy 3500, Smart-UPS VT and ais3000 ... Galaxy 3500, Smart-UPS VT and ais3000 Power Factor Information Resolution : ... The Input Power Factor is 1 . There is no phase shift between voltage and current on the input, which minimizes the installation costs by enabling the use of smaller size cabling.


Résultats 1 - 10 de 66

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.