Consulter la FAQ



Technical Spec’s on a acpa4000
Resolution : ... 60% 8257 kW Kw ... Power Consumption ( kW ) 1.6 kw /hr is ... Plug CFG NEMA 5 -20 Min ... ... (CFM) 400 low/ 600 high Condenser Fan ... typical is 3.8a Air Differential switch Factory setting . 8 ... restart to prevent damage Automatic Restart Yes If power is cut unit will return to last known operating condition upon power up Programmable Thermostat Yes Control Panel Yes Programmable Schedules Yes Key Features ... Operating Cost per hour ($.14/ kW ) $
Spare parts list for ACRD1XX, and ACRD2XX
Resolution : ... DOOR ASSY 10 KW - SPARE PART 9. 600 195.0 ... ... 380.0 5 .450 69 ... w0p2570 CRAC 8 X 2 FORM- ... ... " STRAIGHT C X C - SPARE ... 3/ 8 " ODF - ... 1/2"ODM X 5 / 8 " ODF EXTENDED, r410a 3 TON - SPARE PART 0.656 160.0 160.0 160.0 0.561 160.0 110.0 85
APC Schneider Cooling Unit Identification
Resolution : Capacity KW MA= 600 /3/ ... X = No Reheat ... X =No Humidifier ... Capacity KW MA= 600 /3/ ... EA= 600 /208/ ... X = No Reheat ... X = No Humidifier ... Capacity KW MA= 600 /3/ ... EA= 600 /208/ ... X = No Reheat ... X = No Humidifier ... Capacity KW MA= 600 /3/ ... EA= 600 /208/ ... X = No Reheat ... X = No Humidifier ... Capacity KW ... AFX 018 ( 5 T) MA= 600 /3/ ...
Network Air FM unit spare parts list
Install Resolution : ... 12R 7/ 8 "SWT ... 14R 7/ 8 "SWT ( ... ... ASSY FM 35 KW DX ... ASSY FM 40 KW DX ... ASSY FM 50 KW DX ... UF & DF 5 /Unit 756 X 325 X 102mm (29.7 X 12.8 X 4IN) ... UF & DF 5 /Unit 756 X 325 X 102mm (29.7 X 12.8 X 4IN) ... FM35-50 KW W/AIR ... ... FM35-50 KW W/AIR ... ... FM35-50 KW W/AIR ...
NetBotz TFTP upgrade/recovery procedure
Resolution : ... Due to antivirus programs setting the tftpd32 ... ... use any tftp program , or if ... tftpd32.exe program , see . ... /4. X . X /tftp/ ... 5 ) Connect a ... ... : 38, 400 ... Data Bits: 8 8 ) When opening ... Wait 5 seconds and plug ... ... the TFTP server installed and running) 17) Issue the following command: rootupg <enter> This process will take approximately 7- 8 minutes to complete. ... You should now be able to manage the NetBotz Appliance using the application .
How to enable .NET 2.0 on Windows 8.x and 10
Windows 8 . x and 10 ... .Net 2.0 is not pre- installed as part of the OS ... You will need to install the .Net 3.5 ... 3. Go to Programs and features ... 5 . You should see .NET Framework 3.5 (includes .NET ... Framework 3.5 and click ok. Windows will proceed to install the service (downloading it from windows update if necessary). ... 2.0 you can now install PowerChute Personal Edition 3.0.2
Things To Consider When Upgrading or Downgrading a Network Management Card 2 (NMC2) Device between v5.X.X and v6.X.X
All serial numbers All installations of v6. X . X firmware with the aforementioned applications
Video: Data Center Expert | Desktop Client Requirements, Download, & Installation
... Expert desktop client software ? ... to download and install the client application to your local ... Resolution : ... discusses downloading and installing the Desktop Client ... Data Center Expert software . ... -alone Java application that runs on ... ... 7, Windows 8 , or Windows ... Screen resolution should be set ... at least 1024 x 768. ... Desktop Client ( application ). 5 ) Run the ... 6) Once the installation completes, you can launch to the Desktop Client using the Desktop Icon (if done during installation ) or the Start Menu Option for StruxureWare Data Center Expert #.#.#.
Why is the Environment Tab missing from the web interface on my AP9631 NMC2 v5.X.X firmware?
The firmware application is incorrect for the product that the AP9631 is installed in.
Creating an Aggregate Device within the KVM Access Software
... KVM Access Management Software and why it ... KVM Access Software (ships with ... ... their KVM Access Software All software versions ... through the Access Software . When a ... ... 300 servers and 600 PDU ports/ ... Resolution ... the KVM Access Software . 5 .) Optional ... 8 .) Fill ... ... , Dell DRAC 5 , Dell iDRAC ... SPM ( Service Processor Management) ... ... , Dell DRAC 5 , Dell iDRAC ... 5 .) When you return to the Port List page, the selected ports are automatically unlocked and are listed as being associated with the Aggregate Device. ... Additional Notes and FYIs: Power port numbers can not be greater than 8 .


Résultats 1 - 10 de 90

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.