Consulter la FAQ



Where can I view community resources and documentation for Data Center Operation?
... .exchange.se.com/t 5 / EcoStruxure - IT -forum/bd-p/ ecostruxure - it -forum
Data Center Expert | What virtualization environments are supported?
The most recent information on supported virtualization platforms can be found within the EcoStruxure IT Help Center at: ... The full-featured demo of the virtual appliance monitors up to five device nodes and one surveillance node . You can purchase a license key to upgrade to a production version to monitor additional device nodes and activate supported applications, or to migrate from a server hardware version to a virtual appliance.
Data Center Expert | How do hardware and software support contracts work?
... come with 2 years of factory hardware ... ... a default 25 nodes (covered under ... as each additional node license. ... a total of 5 years , which includes 2 years of factory warranty ... Year 1 Year 2 Year 3 Year 4 Year 5 Year 6 ... virtual appliance until it is activated using ... ... amount of Device Nodes Installed ... all of the Node Count (column ... ... the base 25 nodes installed on the ... 1 Year Software Support SKU 3 Year Software Support SKU ... ) Take the node count determined above ... Amount of Device Nodes Installed and subtract 25 nodes from the total ...
Data Center Expert | Trial version VM appears to have 25 nodes available.
This is by design. It was done so APC did not need to add a 5 node key to just this one version.
Creating an Aggregate Device within the KVM Access Software
... Software and why it may be suggested ... ... ships with KVMXXXX Digital IP KVMs) ... wishing to consolidate nodes within their KVM ... ... as a single node , and only ... ... together, making it easier for the ... ... I have 300 node license but have ... ... purchase a 900 node license to cover ... effectively creating 150 nodes in total. ... ... the amount of nodes I need to ... ... to connect to it (via browser ... 5 .) Optional ... If it has more than ... ... , Dell DRAC 5 , Dell iDRAC ... ... will bring up its management page. ... , Dell DRAC 5 , Dell iDRAC ...
UPS Network Management Card 2 (NMC2) Certain Events do not work properly with the Dry Contact I/O Accessory (ap9810) Control Policy
... design change to allow this will be evaluated for future firmware ... properly for v 5 .X. ... output relay to it's normal state.
PowerChute Business Edition Agent fails to connect using simple signaling on RHEL 5.x due to SELinux access policy
OS: Red Hat Enterprise Linux (RHEL) 5 .x x64, x86 Build: PowerChute Business Edition 9.1.1 and 9.0.3 OEM Basic and 25 Node Deluxe ... The policy forbids a library used by the PowerChute Agent from running in its current context.
New demo available: IT Expert and EcoStruxure IT app
IT Expert demo https://ecostruxureit.com A self-service product demo that replicates the EcoStruxure IT Expert experience is available on .
SmartConnect Portal indicates that the firmware is out of date on my SmartConnect enabled UPS. How do I update it?
... SmartConnect enabled ( EcoStruxure ™ Ready) ... EcoStruxure ™ Ready Smart ... EcoStruxure ™ Ready Smart-UPS products are able to download the latest UPS Firmware from the Cloud. ... https://www.smartconnect-support.apc.com/help/EN/index.html#page/ EcoStruxure %2520ready%2520smart-UPS%2520help%2520center%2fmn04.6.2.html%23 ... The update will take approximately 5 minutes to complete from the time you initiate the update.


Résultats 1 - 10 de 78

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.