Consulter la FAQ



Where can I view community resources and documentation for Data Center Operation?
... .exchange.se.com/t 5 / EcoStruxure - IT -forum/bd-p/ ecostruxure - it -forum
Data Center Expert | What virtualization environments are supported?
The most recent information on supported virtualization platforms can be found within the EcoStruxure IT Help Center at: ... The full-featured demo of the virtual appliance monitors up to five device nodes and one surveillance node . You can purchase a license key to upgrade to a production version to monitor additional device nodes and activate supported applications, or to migrate from a server hardware version to a virtual appliance.
Data Center Expert | How do hardware and software support contracts work?
... come with 2 years of factory hardware ... ... a default 25 nodes (covered under ... as each additional node license. ... a total of 5 years , which includes 2 years of factory warranty ... Year 1 Year 2 Year 3 Year 4 Year 5 Year 6 ... virtual appliance until it is activated using ... ... amount of Device Nodes Installed ... all of the Node Count (column ... ... the base 25 nodes installed on the ... 1 Year Software Support SKU 3 Year Software Support SKU ... ) Take the node count determined above ... Amount of Device Nodes Installed and subtract 25 nodes from the total ...
Runtime Calibration feature requirements for SMX/SMT units
... working properly, it is either refused ... ... required load is 10 % (SMX ... %; with 5 or more XBPs ... It is recommended not to perform more than one or two runtime calibrations per year , as frequent battery calibrations can significantly decrease the life expectancy of the battery. ... It is important to note that the actual run time during a power outage is not affected by whether a run time calibration had been performed, as the actual run time is dependent on the physical power
Creating an Aggregate Device within the KVM Access Software
... Software and why it may be suggested ... ... ships with KVMXXXX Digital IP KVMs) ... wishing to consolidate nodes within their KVM ... ... as a single node , and only ... ... together, making it easier for the ... ... I have 300 node license but have ... ... purchase a 900 node license to cover ... effectively creating 150 nodes in total. ... ... the amount of nodes I need to ... ... to connect to it (via browser ... 5 .) Optional ... If it has more than ... ... , Dell DRAC 5 , Dell iDRAC ... ... will bring up its management page. ... , Dell DRAC 5 , Dell iDRAC ...
What are the factors that affect Battery Rated Service Life?
On paper, batteries are given a design life of 5 years , 8 years , 10 years , etc. They get weak, ...
Why are the Trigger Alarm and Run Self Test buttons grayed out for my unit on the SmartConnect web portal?
Once the change has been made it will take a 5 to 10 minutes for the change to take affect and the web browser will ...
Why isn’t snmpv3 working properly in Network Management Card AOS versions 3.5.7 and earlier?
Upon rebooting, the NMC will take about 5 - 10 minutes to complete its backend processes needed in order to enable snmpv3.
Frequently Asked Questions for the new Lithium-ion Smart-UPS products.
Is it safe to use ... Cycle life refers to the number of times a battery can expect to be fully discharged and recharged within a specified temperature range before it needs to be replaced. ... The UPS warranty is 5 years for both the electronics and the internal batteries. ... So it is possible to replace the internal batteries while the UPS is operating in online mode. How likely is it that I will need to replace my batteries under normal circumstances? ... The lifecycle of the UPS is approximately 10 years . ... It is recommended that the UPS be replaced with a new model.


Résultats 1 - 10 de 78

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.