Browse FAQs



Frequently Asked Questions (FAQs) for UPS Network Management Card 2 (NMC2)
Is UPS NMC 2 compatible with all single phase SmartSlot UPSs Does UPS NMC 2 integrate with StruxureWare Data Center Expert and InfraStruxure Manager?
Data Center Expert | Why does the trap I received omit the argument for sensor ID?
StruxureWare Data Center Expert NMS integration feature. 7.x and prior.
Netbotz Advanced View | Does NOT Support Radius, Active Directory or LDAP
NOTE: NetBotz Central, ISX Central, and StruxureWare Data Center Expert do support integrating with both Active Directory & OpenLDAP remote authentication server ...
Why does StruxureWare DCE show duplicate sensors after upgrade, one of the duplicates reports unplugged.
... the DDF are at times necessary in order to better integrate the sensor information with external systems such as StruxureWare Data Center Operation.
What type of information is provided in an SNMP trap from StruxureWare Data Center Expert?
StruxureWare has the ability to send traps using the "Alarm ... " functionality as well as the "Network Management System Integration " feature.
Can StruxureWare Data Center Expert be configured to alert for NetBotz 3xx, 4xx, and 5xx devices?
Ever since their integration with NetBotz Central, NetBotz devices were designed to alert for themselves.
Data Center Expert | How do I enable SSL communication between StruxureWare and multiple Netbotz devices?
integration , swc, isxc, dce, cert, ssl, netbotz, botzware, bot, certificate, ssl
Why doesn't StruxureWare or ISX Manager's mass configuration feature update or show password credentials on APC Network Management Card devices?
... ISX Manager or StruxureWare may not work ... ... devices with an integrated card), ... In NMC2 (ap9630, AP9631, AP9635, or any devices with an integrated card) v5.X.X, the passwords are also not stored in this configuration file. ... The config.ini file could be manually configured outside of ISX Manager to include the password using the information from the [SystemUserManager] section above. ... If you have ISX Central or StruxureWare Data Center Expert, this should not be an issue.
StruxureWare Data Center Expert message stuck retrieving configuration
Issue: StruxureWare Data Center Expert message stuck retrieving configuration after pushing a configuration to an SNMP device.
How do I add a DDF to StruxureWare Data Center Expert?
Issue: How do I add a DDF to StruxureWare Data Center Expert?


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.