Browse FAQs

Lighting calculation for Lighting Kit part numbers; ACDC2018, ACDC2019

Published date: 20 August 2020

Can Schneider Electric provide lighting calculation files (.ies)? The customer is trying figure out a way to show adherence to our standards with the lighting used in the containment units. We have to have a minimum of 50 foot candles at all racks/cabinets.

Schneider-Electric does not provide such .ies files, however attached is the photometric specs needed.  The document gives the footcandles at various locations.  Note that if frosted lens are used, a .75 multiplier must be applied. There are qty 4 in the ACDC2018, qty 6 in the ACDC2019

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.