How to change the log off delay of the PowerChute Business Edition web page?
Published date:
20 April 2020
Issue:
The log off delay of the PowerChute Business Edition web page is to short or too long.
Product:
PowerChute Business Edition version 10
Environment:
All supported OS
Cause:
Informational
Solution:
For Windows OS when installed to the default page
Go to C:\Program Files (x86)\APC\PowerChute Business Edition\agent\etc and save the file webdefault.xml to Saved-webdefault.xml Once the file has been saved open webdefault.xml with a text editor. Search for the line session-timeout.
<session-timeout>15</session-timeout>
Change the 15 to the timeout you would like and save the file. Example: change 15 to 30 for the timeout to equal 30 minutes. Then open a command prompt as an administrator and enter the command net stop apcpbeagent Wait for the service to stop then enter net start apcpbeagent and the service will restart. The new timeout delay will now be in affect.
For Linux OS when installed to the default path
Go to /opt/APC/PowerChute Business Edition/agent/etc and save the file webdefault.xml to Saved-webdefault.xml Once the file has been saved open webdefault.xml with a text editor. Search for the line session-timeout.
<session-timeout>15</session-timeout>
Change the 15 to the timeout you would like and save the file. Example: change 15 to 30 for the timeout to equal 30 minutes. Then restart the PowerChute service. The command is sudo systemctl restart PBEAgent
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.