Technical FAQs

Ask a Question

How do I serially connect to the NetBotz 750?

Issue:

How do I serially connect to the NetBotz 750?

Product Line:

NetBotz

Environment:

NetBotz 750 serial port configuration and driver

Cause:

The NetBotz 750 uses a different serial port driver than the older version 3 NetBotz 3xx, 4xx, and 5xx units.

Resolution:

The NetBotz 750 uses the following serial parameters:
Baud Rate - 115200
Data Bits - 8
Parity - None
Stop Bits - 1
Flow Control - None

To log in and configure the 750 with an IP, you will need to log in with root as the user and you will be prompted for a password.

If you connect your NetBotz 750 to your computer and do not see it show up as a serial port (unknown device), you need to download the driver:

Serial port driver - Silcon Labs CP2103
https://www.silabs.com/products/development-tools/software/usb-to-uart-bridge-vcp-drivers
Was this helpful?
What can we do to improve the information ?