Technical FAQs

Ask a Question

NetBotz 4.6.3 e-mail "From" address shows as "Unknown"

Issue:

NetBotz 4.6.3 e-mail "From" address shows as "Unknown"

Product Line:

NetBotz

Environment:

NetBotz version 4.6.3 firmware

Cause:

A change was made to the e-mail process which appears to have broken the "From Address" when you receive an e-mail alert action. If you test e-mail from the e-mail server applet, the from address appears correctly in the received e-mail.

Resolution:

This issue should be resolved in the next Netbotz firmware or "BotzWare" release.

It is not usually recommended that customers downgrade their appliances but if you want to revert to a previous firmware revision, please see k-base FA367489
Was this helpful?
What can we do to improve the information ?