Browse FAQs



APC Schneider Cooling Unit Identification
APC Cooling Unit identification. All Cooling Units . APC Unit Identification ... Expansion A= Air Cooled E= Air Cooled ... W= Water Cooled ... F= Water Cooled ... D= Water Cooled ... G= Glycol Cooled ... B= Glycol Cooled ... P= Glycol Cooled U= Upflow R= Upflow ... coil C= Chilled Water U= Upflow R= Upflow C= Chilled Water ... Main C= Chilled Water ... Main A= Air Cooled ... W= Water Cooled ... G= Glycol Cooled BA=208 ... U= Upflow ... ) A= Air Cooled ... W= Water Cooled
Why do I need refrigerant traps in my piping?
All Air Cooled Cooling Units ... Data Center Cooling ... A: Whenever a condenser is located above the compressor, an inverted trap or check valve should be installed at the condenser inlet to prevent liquid refrigerant from flowing backwards into the compressor during off cycles.
What are the operational conditions for an InRoom (Stulz) Unit
... (Stulz) Unit . ... precision air conditioning units operate within the ... Chilled water-/ cooling water pipes: ... piping between the cooling unit and the air cooled condenser: 60 ... ... condenser and the cooling unit : 5 m ... is below the cooling unit Cooling fluid (DX): 30% Glycol ... Chilled water medium (CW): 0% Glycol ... Downflow units with an external static pressure: 20 Pa (0.08 in w g) Upflow units with an external static pressure: 50 Pa (0.20 in w g)
What are your condenser clearances and placement requirements?
All Cooling Condensers Data Center Cooling ... the location of air-cooled equipment is the ... Units must not be ... ... is that the unit should be mounted ... Units should be mounted ... ... to properly protect fan decks and piping ... and damage the unit or piping. Height Requirement ... feet above the unit providing all other ... Walls or Obstructions The unit should be located ... ... sides of the unit should be a ... When the unit is in an ... three walls the unit must be installed as indicated for units in a pit ... Multiple Units For units placed side by ... minimum distance between units is the width of the largest unit .
DAC, Cancoil Installation Manual
Air Cooled Condenser DAC Air Cooled Condensers For information ... Cancoil air-cooled condensers have been ... ... provided in the unit . DO ... SECTION OF THE UNIT . Unit Placement and Mounting ... ... be used if air-cooled quipment is located ... unit should be securely ... ... clearance around the unit for proper servicing ... Cancoil air-cooled condensers are available ... variety of optional fan cycling controls, however many units are shipped without fan controls. Check the unit wiring diagram for ... ... Before starting the unit , check all ... ... % of the unit nameplate voltage.
What does “Equivalent Pipe Length” mean?
Product line: All air cooled cooling units .
What is the power factor (PF) of the ACSC cooling unit?
Most of the PF comes from the compressors. The unit fan power bus rectifiers are PF corrected.
Network Air FM fan curve chart
Issue: Network Air FM fan curve chart.
Can I use Type L soft copper for my installation?
Product line: All Air-Cooled Cooling Units


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.