How can I mass configure a Network Management Card (NMC) or NMC embedded product?
How can I mass configure a Network Management Card (NMC) or NMC embedded product? ... can I mass configure or configure multiple Network Management ... ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... , ap9340, NetBotz 200) ... AP9312TH, MasterSwitch 1 /2) ... ... Card, mass configuration of those devices ... ... and uploading a single configuration file ( config .ini) ... ... modified through the config .ini ... , these four settings will be disregarded ... ... keyword will not configure Output Voltage, ... ... I obtain a config .ini ... file from a single Network Management Card ... ... firmware versions, one option is to retrieve the config .ini