Consulter la FAQ



Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
... such as a Rack PDU, AV ... ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... ... UPS Online ( SRT ). ... AP9635, and Rack PDU 2G ... ... the file a line for each firmware ... On a Rack PDU specifically, ... ... an SCP command line to transfer the ... 3. Use a similar SCP command line , with the name of the application module, to transfer the application firmware module to the Management Card. ... Use an SCP command line to transfer the .nmc3
How to select SSL/TLS cipher suites on Network Management Cards
Devices with an embedded Network Management Card 2 include (but are not limited to): 2G Metered/Switched Rack PDUs (AP84XX, AP86XX, AP88XX, AP89XX), Rack Automatic Transfer Switches (AP44XX), Certain Audio/Video Network Management Enabled products, Smart-UPS Online ( SRT ). ... Via the NMC command line :
Video: How can I download Event, Data, Configuration, and Debug files from my Network Management Card?
... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... UPS Online ( SRT ). ... via the Command Line Interface (CLI ... Generally, you'd use the cd command in most command line tools. ... Network Management Card 2 (ap9630/31/35) v6.0.6 and higher, Network Management Card (ap9640/41) - How to Export "Debug File Download" via Command Line Interface
What are some features I need to be aware of while manipulating the config.ini file of a APC Network Management Card?
... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... The config.ini file on every network management card can be downloaded using command line FTP or SCP. ... On newer generation Micro-link UPS devices, such as SMX, SMT, SRT , and SURTD the following keywords in config.ini are protected by UPSOverride:
ACRP1XX, ACRD5XX, ACRP5XX, and ACRC5XX Parts List
... 13 FT ( RACK INLET ... KEY) ( Rack ) w0h- ... BLK SX ( Rack ) w0h- ... QUICK CPLR HFC35 IN- LINE HOSE SHUTOFF 1/2 ID (Condensate ... ) 530-1138A WIRE ASSY FM 208v JUMPER 0w2540 WIRE ASSY FM 208v JUMPER SET w0h-0152 WIRE ASSY FM 230v JUMPER 0w2541 WIRE ASSY FM 380v JUMPER 0w2542 WIRE ASSY FM 400v JUMPER 0w2543 WIRE ASSY FM 415V JUMPER 0w2544 WIRE ASSY FM 460v JUMPER [PART OF SHIP LOOSE KIT] 0w2545 WIRE ASSY FM 480v JUMPER 0w2546 WIRE CLIP - BLACK ... HUMIDIFIER SUPPLY LINE CONDENSATE DRAIN LINE
Network Management Card (NMC) Password Reset Procedure
... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... UPS Online ( SRT ). Rack PDU (AP84XX ... 1st Generation Rack Automatic Transfer Switch ... 2nd Generation Rack Automatic Transfer Switch ... 4th Generation Rack Automatic Transfer Switch ... Rack Air Removal Unit ... Rack PDU 1G ... 1st Generation Rack Automatic Transfer Switch ... 2nd Generation Rack Automatic Transfer Switch ... 4th Generation Rack Automatic Transfer Switch ... Rack Air Removal Unit ... ... access the command line interface. ... At the Command Line Interface, use ...
Video: How do I configure APC Network Management Card network settings?
... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... UPS Online ( SRT ). ... AP78XX or AP79XX Rack PDU, Environmental ... ... AP8XXX Next Gen Rack PDU (NMC2 ... ... SMX, and SRT Models with NMC2 ... Rack PDU (AP78XX ... 1st Generation Rack Automatic Transfer Switch ... 2nd Generation Rack Automatic Transfer Switch ... 4th Generation Rack Automatic Transfer Switch ... Rack Air Removal Unit ... Rack PDU 1st Generation Rack Automatic Transfer Switch ... 2nd Generation Rack Automatic Transfer Switch ... Rack Air Removal Unit
Can I use a 230v Smart-UPS in a 277v environment?
Environment: All Line Interactive 230v models, All Serial Numbers
How to check if the PowerChute Business Edition Agent daemon is running on Unix/Linux systems.
... is not running or not running normally, the command will only return one line that stands for the grep process itself.
How to check if the PowerChute Network Shutdown daemon is running on Unix/Linux systems
... is not running or not running normally, the command will only return one line that stands for the grep process itself.


Résultats 1 - 10 de 50

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.