Consulter la FAQ



Can the NetShelter SX cabinets be bayed with the side panels on, and how do the baying brackets work?
All versions and serial ranges . ... The design of the NetShelter SX baying hardware allows for a single cabinet with equipment installed to be removed from a row. The baying of cabinets with side panels in place offers several advantages to end users. First and foremost, front to back cooling air flow is enhanced by the use of side panels.
Why Node-red embedded with Ecostruxure Augmented Operator Advisor stop few second after starting?
How to diagnotic When you start AOA, there is one MS-dos windows with a lot of information
Can cable bridge partition/trough be installed across the top of a 300 mm or 600 mm InRow chilled water cooling unit?
The NetShelter cable partition won't install on top of the InRow cooling unit . ... NetShelter, InRow Cooling , Row Power Distribution ... All versions and serial ranges . ... There are no square holes in the roof of the 300 mm chilled water cooling units so there's nowhere to connect the tabs on the NetShelter cable partition. ... A NetShelter trough such as ar8580 or AR8561 may also be used to span the cooling unit but they can not be attached directly to them. NetShelter troughs can span one cabinet width without attaching directly to the cooling unit roof.
Are the fans in a 600mm Cooling unit single phase or 3-phase?
Issue: Are the fans in a 600mm Cooling unit single phase or 3-phase?
What are some of the applications for the InRow ACRD?
InRow Cooling ... install the same unit in different applications ... ... building new IT assets are looking to replace old legacy cooling methods with newer ... ... with its wide range of capacities and ... of close coupled cooling . ... platform, new cooling problems arise in ... ... for more predictable cooling in this new ... ~ As the load change, the demand for cooling will increase. Typical data center cooling looks at the temperature of the room to adjust capacity. ... The InRow RD is controlled via multiple modes using a rack inlet temperature probe, which enables quick response to changing demands, thus protecting expensive IT assets .
How to navigate through an Network Air FM unit display
... Network Air FM unit display. Only qualified service personnel should make ... ... , then the cooling setpoint is used ... ... work as a single System. ... Half capacity uses one compressor and half ... ... avoid over- cooling while dehumidifying. When the unit is in dehumidification ... ... the modes ( cooling , reheat, ... ... compressor (stage 1 ) in a ... ... there is no cooling demand. ... times of no cooling demand in applications ... ... a demand for cooling , the Economizer ... ... a demand for cooling , the Economizer ... event to one of the output ... ... is the sensitivity range above the
What are the operational conditions for an InRoom (Stulz) Unit
This document will describe what are the operational conditions for an InRoom (Stulz) Unit . ... The InRoom precision air conditioning units operate within the following ranges : ... Frequency:60 Hz +/- 1 % Chilled water-/ cooling water pipes: ... Maximum equivalent length of piping between the cooling unit and the air cooled condenser: 60 m (200 ft) Maximum level difference between the condenser and the cooling unit : 5 m (16 ft) when the condenser is below the cooling unit ... Cooling fluid (DX): 30% Glycol
How to set up group communications for an Network Air FM unit
1 ) Please locate ... of the FM unit [Figure 1 ] and land ... connects the next unit in the group ... 1 Figure ... . Please select one of these configurations ... ... number of FM units in the system ... ... alarm occurs in one System. ... alarm occurs in one System. 4.Please set the group configuration cooling load-sharing and System role-assignment functions ... If the environmental temperature or humidity is outside the range determined by the setpoint and threshold, the System will generate a load-sharing request. ... However, acceptable ranges for each mode are:
What filter is being used for your InRow 300mm?
InRow 300mm Units ... Data Center Cooling ... The system uses a <20% efficiency ASHRAE 52.1, 12.7 mm ( 1 /2 in) washable, deep loading, large dust-holding filter that meets HF- 1 standards for electronics (MERV 1 per ASHRAE 52.2). ... 1 acrc10x ... various voltage range
Why choose glycol over water?
All cooling units that require heat exchangers ... Advantages of Glycol: ... - Did you know that just 1 /16" of scale reduces heat transfer by 40%! ... - In cooling systems where components are frequently disconnected and reconnected, the glycol is typically captured and added back to the system.


Résultats 1 - 10 de 98

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.