Consulter la FAQ



What are the various generations of Smart-UPS Products?
Current Products: " SMX " (IE: smx1000) ... 750va - 3kva ... Fully interactive LCD display All units Rack / Tower convertible ... High efficiency “ green ” mode ... Simplified LCD display ... High efficiency “ green ” mode ... All units are Rack /Tower convertible ... Rack / Tower or Rack / Stack convertible ... LCD Display Rack / Tower or Rack / Stack convertible
Video: How do I configure APC Network Management Card network settings?
... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... ... AP78XX or AP79XX Rack PDU, Environmental ... ... AP8XXX Next Gen Rack PDU (NMC2 ... ... UPS front panel LCD - (available ... supported SMT, SMX , and SRT ... ... have a solid green status LED. Rack PDU (AP78XX ... 1st Generation Rack Automatic Transfer Switch ... 2nd Generation Rack Automatic Transfer Switch ... 4th Generation Rack Automatic Transfer Switch ... Rack Air Removal Unit ... Rack PDU 1st Generation Rack Automatic Transfer Switch ...
Frequently Asked Questions for the new SMX and SMT series of Smart-UPS products.
... regarding the new SMX and SMT series ... ... UPS SMT and SMX ... The SMT and SMX series of Smart ... UPS Frequently Asked Questions New Smart-models are identified by their intuitive LCD interface. These models also have part numbers that start in the prefixes “ SMX ” and “ ... How does the ‘ green ’ operating mode increase efficiency? ... APC’s patent pending ‘ green ’ mode bypass components that perform automatic voltage regulation (AVR) when not needed. ... To use earlier versions of software requires an optional SmartSlot , the ... What mounting hardware is provided with the SMX units?
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
... such as a Rack PDU, AV ... ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... ... AP9635, and Rack PDU 2G ... ... removable NMC2 UPS SmartSlot card, you ... into the UPS SmartSlot , effectively rebooting ... On a Rack PDU specifically, the LCD display will show ... ... Card in the SmartSlot , then immediately ... Card in the SmartSlot , then immediately ... seconds turns solid green or slowly flashing ... LED turns off and after 20 seconds turns solid green or slowly ...
Smart-UPS C Series FAQ
Is the LCD display the same ... on SMT and SMX Smart-UPS ... ... , the SMC LCD display is a ... SMC rack mount units ship with a rack mount brackets that ... and 4 post racks . It can ... or threaded hole racks without modification. ... a 4 post rack can purchase a 4 post rack mount rail kit ... ... efficiency "" green "" mode ... ... setting from the LCD interface? How do I turn off the LCD display? ... To activate LCD Power Saving Mode: ... LCD will now go dark after 60 seconds of no activity LCD will light when an event occurs or a button is pressed
AP84XX, AP88XX, AP89XX, and AP86XX 2G Rack PDU LCD Backlight Behavior
In the green and white interface, navigate to About->RPDU.
How do I properly install/uninstall my SmartSlot accessory card into my UPS?
... /uninstall my SmartSlot accessory card into ... ... /removing a SmartSlot accessory card typically ... connector of the SmartSlot accessory. ... most situations, SmartSlot cards can be ... bottom of the SmartSlot connector. ... Generic reference showing SmartSlot connector with 24V ... If your SmartSlot accessory looks similar ... this identifies the SmartSlot accessory as hot ... ... side of the SmartSlot connector. ... orientation verifies the SmartSlot accessory is hot ... ... and install the SmartSlot card while the ... ... the accessory or SmartSlot for some reason ... ... flash its front LCD . ... or install a SmartSlot accessory card and ... ... -UPS ( SMX /SMT)
Why can I not adjust output Voltage on my SMX "LV" or "HV" series Smart-UPS?
... output voltage on SMX "LV" ... SMX "LV" ... ... Smart-UPS SMX units with " ... ... , 220v, 230v , or 240v ... ... using either the LCD screen on the UPS ... On the LCD interface the option is not shown in the menu until output is turned off. ... Turn output power OFF via the LCD screen or Network Management Card interface. ... Once the UPS output is turned off, you can adjust output power via the "Configuration" menu on the LCD screen or Network Management Card web interface. If using the LCD screen , you must first enable Advanced menus.
UPS Interface Expander 2 SmartSlot Card (AP9624) - Incorrect System Behavior for Some Master Server Control Functions
... from the UPS's LCD . ... For SMT, SMX , and SRT ... ... from the UPS's LCD . ... or from the LCD in these systems ... SMT Tower (firmware UPS 08.0 or greater) UPS 09.3 SMT 2U Rackmount UPS 09.3 SMT 1U Rackmount (follow " SMX 1500va or less" firmware) UPS 09.8 SMX 1500va or less (firmware greater than UPS 05.0) UPS 09.8 SMX Larger than 1500 VA (firmware between UPS 05.0 - UPS 07.0
Why is my Rack Automatic Transfer Switch inaccessible after a firmware upgrade?
My Rack Automatic Transfer Switch (ATS) inaccessible over the network after a recent firmware upgrade. ... Rack ATS models: ... These models can be quickly identified by their UPS-like SmartSlot - their Network Management card is removable. ... APC has (2) current generations of Rack ATS products that use two different firmware revisions. ... These models can be quickly identified by their UPS-like SmartSlot - their Network Management card is removable. ... They are easily identified by their unique LCD display and built-in network jack.


Résultats 1 - 10 de 50

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.