Consulter la FAQ



Where can I get support for APC and MGE Products?
... 10 0031- 6 0033-10 ... 50 0033- 6 0034-1 ... ... 3 0423- 6 0429-25 ... ... 3 0507- 6 0527-2 ... ... 75126 1089- 6 1098-10 ... 10 1124- 6 1135-10 ... 25 1135- 6 1190-10 ... 25 1193- 6 1195- 6 12000-10m ... ... 15 1439- 6 1443-1 1443- 6 1503-10 ... 3 1504- 6 1586-10 ... ... 3 1683- 6 1686-1 ...
Smart-UPS C Series FAQ
... Smart-UPS C Series FAQ ... Smart-UPS C series? ... Smart-UPS C series is our ... What plug type do SMC models ... ... with a " C " suffix ( ... All SMC units have both a USB port and a RJ-45 style Serial port, only a USB cable is included with the product. A ... Models with a " C " suffix (IE: smc1000c, smc1500c) also include an ethernet port for Smartconnect Cloud Connectivity ... What is the Warranty for "" C "" Sseries Smart-UPS? ... - Press and hold the Power Button for 6 seconds
USB Specifications for the WallBotz 500
USB Specifications for the ... USB specifications. WallBotz 500 USB Specifications 6 USB ports 4 USB channels ... points (internal USB ports) share a USB channel USB ports A & ... USB port C has a dedicated ... USB port D has ... USB options increase the length that USB devices can be from the USB host: USB Cables Attach USB devices to USB hosts/hubs USB Hubs Use standard USB cables to chain ... USB Repeaters / Extenders USB cable with integrated ... ... together with standard USB cable on the ... going to the USB device (80 ... ... the range of USB devices using existing ...
What are the operational conditions for an InRoom (Stulz) Unit
... Between 18° C (64° ... and 27° C (81° ... ... -10° C (14° ... 208- 230v / 3ph / ... ... +42° C (-4 ... +107. 6 °F) ... : 24° C (75° ... ... : 24° C (75° ... ... : 7° C (44. ... ... : 12° C (53. ... ... : 45° C (113° ... ... : 60° C (140° ... ... : 30° C (86° ... Fluid outlet temperature (G): 40° C (104°F)
NetBotz TFTP upgrade/recovery procedure
... procedure are the USB console cable and ... ... ) Connect a USB cable from your ... 6 ) To find ... ... will be a USB Serial port with ... If the USB Serial Adapter is ... 1) Under Session, change the connection type to serial. ... 1) Type a name for the connection and on the next screen select the appropriate COM port that was discovered earlier ... c ) printenv <enter> (print the settings to the screen for verification) ... c ) setenv netmask aaa.bbb.ccc.ddd <enter> (Subnet mask for the NetBotz Appliance)
NetBotz 250 | Configuring Network Settings
6 ) Select the ... ... ) Select a USB port at the ... ... Connect the provided USB A- USB mini B configuration ... ... -to- USB vritual COM port ... 6 ) Use this ... ... .1, type the following command ... 7) Type reboot. ... 250 with 00 c 0 b7 ... ... 141 00- c 0-b ... ... 141 00: c 0:b ... ... each variable, type a numeric value ... ... .1, type the following command ... 6 ) Type reboot.
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
... X to v 6 .X. ... ... UPS or device type . ... Management Card v 6 .X. ... ... .X or 6 .X firmware ... ... application for your type of device. ... X to v 6 .X. ... Universal Serial Bus ( USB ) 1. ... Universal Serial Bus ( USB ) 1. ... *devices with USB : Some USB flash drives are ... ... Please note, USB may not allow ... ... folder on your USB flash drive called ... ... are supported via USB if the device ... ... for known file types
ACRP1XX, ACRD5XX, ACRP5XX, and ACRC5XX Parts List
... 5 & P 6 ... 5 & P 6 ... .0" C X NPTI ( ... ... 0511 PIPE ASSY 6 INLET RECIVER 0 ... POLY BAG ( 6 " X 9 ... ... 5531A SCREW M 6 X 16MM TORX ... ... 0197 t30018 Rev C TYRAP 390mm V ... ... .0" C X NPTI Gasket ... ) 530-1138A WIRE ASSY FM 208v JUMPER 0w2540 WIRE ASSY FM 208v JUMPER SET w0h-0152 WIRE ASSY FM 230v JUMPER 0w2541 WIRE ASSY FM 380v JUMPER 0w2542 WIRE ASSY FM 400v JUMPER 0w2543 WIRE ASSY FM 415V JUMPER 0w2544 WIRE ASSY FM 460v JUMPER [PART ...
Video: Using Network Management Card 2 (NMC2) bootmonitor to recover/upgrade firmware
... .X, 6 .X. ... ... X to v 6 .X. ... ... XMODEM (Steps 6 - 10) ... An USB to serial adapter ... ... on the NMC type the sysinfo ... !!! Type : factory_ ... ... on the NMC type the sysinfo After issueing the xmodem command you should see C ... Browse to the location where you extracted the firmware files in Step 6 , select the bootmon ... firmware file first (if a newer version is available it will be present in the files downloaded in Step 6 ; if the card already has the latest bootmon installed proceed with uploading the AOS
Video: How do I configure APC Network Management Card network settings?
... begin with 00 C 0 B7 ... beginning with 00 C 0 B7 ... ... Cards running AOS 6 .5. ... ... Press Ctrl- C to return to ... ... 0603 micro- USB cable. Type help ... each variable, type a numeric value ... [- c enable | disable ... ... terminal window and type the following ( ... Now, you can Telnet to the card by typing : telnet ... represents the last six characters of the MAC Address (enclosed on a slip with the shipped product) of the NMC. ... APC tests, it took between 6 and 16 minutes before this functionality worked.


Résultats 1 - 10 de 50

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.