Consulter la FAQ



Which accessories/environmental sensors are compatible with my APC Network Management Card (or devices with embedded Network Management Cards)?
... accessories or environmental sensors are compatible with ... ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP86XX ... AP89XX), Rack Automatic Transfer Switches ... ... to the " Sensor " or " ... ... refer to NetBotz sensor compatibility information. Accessories/ Sensors Supported AP9335T Temperature Sensor AP9335TH Temperature / Humidity Sensor AP9335T Temperature Sensor AP9335TH Temperature / Humidity Sensor AP9335T Temperature Sensor AP9335TH Temperature and Humidity Sensor AP9335T Temperature Sensor AP9335TH Temperature / Humidity Sensor AP8XXX series Rack PDU 1/UIO AP9335T Temperature Sensor AP9335TH Temperature / Humidity Sensor
What sensors are supported by the NetBotz Wireless Sensor Pod 180 (nbpd0180) ?
... NetBotz Door Switch Sensor for APC Racks - 12 ft ... NetBotz Door Switch Sensor for APC Racks - 62 in ... NetBotz Door Switch Sensor for Third Party Racks - 62 in ... NetBotz Door Switch Sensor for Rooms or Third Part Racks - 50 ft nbes0302 APC Temperature Sensor - 13 ft AP9335T APC Temperature & Humidity Sensor - 13 ft (Only reports temperature when connected to ... nbpd0180 AP9335TH NetBotz Temperature
APC Environmental Sensors FAQ
We do not officially support lengthening the temperature humidity probe with PS/2 extension cables.
What sensors come with the netbotznbrk0250 ?
Not all sensors are shown in documentation ... Temperature sensors are not shown in the inventory documentation. ... The nbrk0250 comes with one wired universal Temperature and humidity sensor , AP9335TH, and one Wireless Temperature Sensor (nbws100t) Neither are shown in the inventory within the Installation and quick configuration documentation. ... http://www. apc .com/shop/us/en/products/NetBotz- Rack -Monitor-250/P-nbrk0250
How accurate are the APC Environmental Monitoring products?
... accurate are the APC Environmental Monitoring products ... Supported sensors The APC Environmental Monitoring specification sheet states relative humidity (RH) ... ... , the relative humidity measurement can be ... - This means that if the actual relative humidity was 30%, the APC Environmental Monitoring product could read anywhere from 25.5% to 34.5% RH. ... Please keep in mind that these sensors are proximity based, meaning they measure the temperature in a specific location (such as a rack ).
InfraStruXure Central does not read some sensor names if changes are made after initial discovery.
... relay, or temperature / humidity sensor is changed after ... discovery of the APC device, ISXC ... to propagate the sensor name change properly.
After upgrading firmware on my APC AP8XXX series Rack PDU, the input voltage reads 1V
This is due to a firmware issue which typically affects high density AP8XXX series Rack PDUs with high load and high ambient temperature .
Can the NetShelter CX fans be turned on/off, or fan speed raised/lowered, remotely?
Using either NetBotz or a Switched Rack PDU you can control a specific port on the NetBotz or PDU . A temperature sensor can also be used to set thresholds for alarms, or to turn outlets on/off. Please contact your APC Representative to design a solution that suits your particular needs.
NetBotz 250 | Inaccurate Data Logs (prior to v6.4.6 firmware)
... NetBotz 250, temperature and humidity readings may show ... ... 6 the wired sensor temperature values reported through ... Graphing) and temperatures reported through the ... Status > Wired Sensor > Temperature & Humidity ) or the ... Device > Wired Sensor > Temperature & Humidity ) now report the same value if updated at the same time. ... https://www. apc .com/shop/us/en/products/NetBotz- Rack -Monitor-250/P-nbrk0250
NetBotz 750 | Physical Description
- Rack Monitor 750 ... connected devices ( sensor pods, rack access pods, and temperature / humidity sensors with digital displays ... ... NetBotz Leak Rope Sensor (nbes0308) ... 5 Rack Access Ports* ... the door switch sensors (nbes0302 or ... ) and handle sensors (NBHN125 or ... 6 Universal Sensor ports Used to connect APC by Schneider Electric sensors , third- ... dry-contact sensors , and standard ... -5 V sensors . ... -contact state sensors require the NetBotz ... -5 V sensors require the NetBotz ... -5 V sensor cable (nbes0305 ...


Résultats 1 - 10 de 51

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.