{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}
{}

Nos marques

{"support":{"yesButton":"Oui","noButton":"Non","feedback":{"title":"Quelles améliorations pouvons-nous apporter ?"},"submitButton":"Soumettre","successMessage":"Merci de nous avoir fait part de vos commentaires.","title":"Cela vous a-t-il été utile ?","feedbackPercentLabel":"personnes ont trouvé cela utile","captcha":{"error":"Veuillez cocher la case appropriée."}}}
Consulter notre FAQ

Erroneous Fan alarms on the XU1K3LLXXRCC


Issue:

XU1K3LLXXRCC may report erroneous Fan alarms

Product Line:

Smart-UPS Industrial

Environment:

XU1K3LLXXRCC, All Serial Numbers, firmware less than UPS Firmware 2.5

Cause:

Earlier revisions of the UPS Firmware may report erroneous Fan alarms

Resolution:

Upgrade the unit to the latest UPS firmware

UPS Firmware 2.5 introduced improvements to fan status reporting, among other things.
Full release notes are attached to this FAQ.

To upgrade via the Network Management Card refer to FAQ #FA281753
To upgrade via a USB Thumb Drive refer to FAQ #FA402857


You can download the XU1017UPS_02-5.enc firmware image here.
Release notes are attached below.

Pièce(s) jointe(s)

Vous ne trouvez pas ce que vous recherchez ?

Contactez notre service client local si vous avez des questions ou si vous avez besoin de plus de détails ou d'une assistance technique.