{}

Consulter notre FAQ

{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}

Video: How to view alarms on an ACRD200 cooling unit

Issue:
How View Alarms on an ACRD200 Cooling Unit.

Product line:
InRow Cooling Products ACRD200.

Environment:
All Serial Numbers.

Cause:
Install, Configuration

Resolution:



First you need to access the View Alarms menu you can do this by hitting the <ESC> until visible

Then select ENTER

You will be prompted for a Password if limited access is enabled

Use the default password of “apc”

If this does not work check with your Admin for the correct password

If password has been lost use the last eight digits of the serial number

Using the Up and or Down Arrows you can scroll through the alarms


Cela vous a-t-il été utile ?

[tcm:741-234909-217200, tcm:741-309501-217200]