{}

Nos marques

Consulter notre FAQ

PowerChute Network Shutdown v3.1 cannot connect to vCenter Server or ESXi hosts to perform VM and host tasks

Issue:
PowerChute Network Shutdown connects to vCenter Server/ ESXi Host Web Services using the URL "https://<IP Address>/sdk" using TCP port 443. If the TCP port is changed to a non-default port, PowerChute will not be able to connect.

Product Line:
PowerChute Network Shutdown v3.1

Environment:
VMware

Cause:
PowerChute only allows connection using port 443.

Resolution:
Upgrade to PCNS version 4.x
Or
Port 443 must be used.

APC Belgium

[tcm:741-234909-217200, tcm:741-309501-217200]