{}

Consulter notre FAQ

{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}

Physical Sizes of Camera Pod 120 and Sensor Pod 120

Issue:
Physical Sizes of Camera Pod 120 and Sensor Pod 120

Product Line:
NetBotz

Environment:
NetBotz Version 2 camera pod NBPD0121

Cause:
Physical size

Resolution:

Physical Sizes of Camera Pod 120 and Sensor Pod 120

Camera Pod 120
Height (counting jacks on top) = 2.783
Height (not counting jacks on top) = 2.70
Width = 2.625
Depth = 1.090


Sensor Pod 120
Height = 3.863
Width (including temp sensor on the side) = 2.930
Width (not including temp sensor on side) = 2.612
Depth = 1.10

NOTE: The USB cable usually sticks out of the side of the pods about 2 inches.

Cela vous a-t-il été utile ?

[tcm:741-234909-217200, tcm:741-309501-217200]