... / 3ph / 60 Hz ... / 3ph / 60 Hz ... imbalance: < 3 % Frequency: 60 Hz +/ ... ... unit and the air cooled condenser: 60 m (200 ... Return air conditions for evaporator capacity ( DX ): 24°C (75°F) 50% R. H. ... Maximum condensing temperature: 60 °C (140°F) Cooling fluid ( DX ): 30% Glycol ... Data is valid for: 460v / 3ph / 60 Hz ... Upflow units with an external static pressure: 50 Pa (0.20 in w g)
... APC NetworkAIR FM DX Precision Air Conditioner ... • DX ... Direct expansion ( DX ) coil ... —Economizer and DX coils ... water) and DX coils ... the NetworkAIR FM DX 60 Hz Up to three Modules can be ... ... valve which feeds three quarters of the ... ... the NetworkAIR FM DX 60 Hz Installation ... the NetworkAIR FM DX . • DX ... head pressure in DX Systems). —for air-cooled Modules with no ... ... valve as a three -way valve ... ... valves are always three -way valves ... ... valve as a three -way valve ... Air-cooled Systems with no ...