Browse FAQs

What size panel (or range) does the NetShelter cage nut fit?

Published date: 11 November 2019

Issue:
The panel range for NetShelter cage nuts is requested. 

Product Line:
NetShelter SX, SV, VX and WX hardware. 

Environment:
AR8100, AR8005

Cause:
Extra cage nuts are needed and must be sourced locally. 

Resolution:

The NetShelter cage nut panel range is 1.6mm - 2.0mm. This equated to a 14 awg to 16 awg panel. 
All cage nuts provided by APC for NetShelter cabinets use this size, regardless of nut/screw combination. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.